Parker Support Community
  • About the Community

    The Parker Community is a knowledge base for anyone using or interested in using the company's technologies, products, and systems. Read more...

  • Ask A Question

    If you have a specific question, you can ask it here or ask it within the appropriate technology group.

  • Community Terms of Use

    Parker encourages all users of its social media sites, pages, channels and community to communicate and engage in a constructive, meaningful and professional way. Read more...

Latest Blog Posts

Integrated Transmissions That are a Cut Above Turfcare Pump and Motor DivisionThere are over 40 million acres of lawn across the United States, made up, primarily, of residential lawns, roadsides and golf courses. While many Americans maintain their own lawns, a growing number of contractors, landscapers and lawn care consultants are hired to do the job. For these working men and women, the more lawns maintained during the day, the more successful their businesses become. To mow faster and longer, specialized mowers are used to mow more grass with more precision. 

Transmissions: a driving force

As with any machine, a commercial mower’s primary function is to make a task easier, in this case, mowing grass. Via a network of hydraulic, mechanical, electrical and chemical processes, a mower is propelled by a simple push or pull by the operator. One such process is performed by transmissions, located near each wheel of the mower. These integrated drive systems pull power from the engine and create the torque and speed required to get a mower moving and to keep it moving. A combination of a hydraulic pump and motor can also be used if space allows.

For a smooth and comfortable ride, a quality drive system is required. Otherwise, the mower can begin to cog when the drive is placed under too large a load. Cogging can ruin the user experience and potentially result in a stuck mower. Nothing will set an operation back like stuck equipment.

Cogging can create problems for a user as the mower starts to move, but once the mower is in motion, the drive system’s job is not done. To maintain a fast, effective cut, a drive system must provide consistent power throughout a job. UCLA legend John Wooden said, “Be quick, but don’t hurry”. He used this sentiment while coaching his championship basketball teams, but the same can be echoed in the turf industry. Speed is important, but an ineffective cut, caused by an inferior drive system, wastes time.

The gold standard

Parker’s HT Series is the pinnacle of drive systems in the turf industry. By coupling a Torqmotor and variable displacement pump, the HT Series delivers more power to the cutting deck, decreases fuel cost, and eliminates cogging. When used with Parker formulated HT-1000 transmission oil, oil change intervals are increased to 1000 hours; 2x longer than competitive drive systems. Find out more about this efficient drive system at parkerHT.com.

The Pump & Motor Division is a market leader in gear pump and low speed-high torque gerotor motors, that continues to blaze a trail in the industry by developing new technologies while maintaining the high level of service synonymous with Parker. Between its two locations in North Carolina and Tennessee, the division employs decades of industry experience to better serve you and your application.

Attending GIE 2019? Visit us in Louisville, KY October 16 – 18 at booth #10124 to see the HT transmission. 

 

Integrated Transmissions That are a Cut Above CT Lefler Pump and Motor DivisionThis article contributed by CT Lefler, marketing product manager, Pump & Motor Division, Parker Hannifin Corporation.

 

 

 

 

Related articles:

Hydrostatic Transmission Fluid Engineered for Low Maintenance

Simplified Hydraulic Pumps for the Low Speed, High Torque Market

New Dump Pump Revolutionizes the Dump Truck Market with a Small Frame

 

Integrated Transmissions That are a Cut Above

Read more

The ROI of IOT for OEMS - Increased Revenue Service - Parker Mobile IoTThe OEM landscape is continuously transforming. In a service industry that once focused on the tactical side of product function, the new shift now emphasizes on how to become the strategic revenue generator and competitive differentiator through the utilization of modern technological systems, such as IoT. 

This pressure enhances the competitive environment, putting OEMs on a constant mission to expand their offerings and provide the best in class equipment to their customers to build new partnerships and enhance their current relationships. The key metric of this strategy is ensuring customer satisfaction. But we cannot simply neglect the importance of increased productivity, efficiency, and achieving appropriate returns on investment (ROI).

According to Bain’s projections, 6.8 million connected heavy construction machines will be shipped between 2018 and 2025. It is clear that the future largely depends on the Internet of Things (IoT) to power further data collection and analysis and overall innovation in the field. Yet this investment into IoT, like any strategic investment, must be assessed and the ROI is a critical measure before determining whether your organization should invest.

The top performance indicators for measuring the success of IoT for heavy equipment OEMs are:

  • Exceptional customer experience
  • Capture replacement part business
  • Reduction in costs and increase in productivity
  • Service compliance and increased service traffic
  • Reduced development costs

Let’s take a look at how IoT can enhance an OEM's performance in these specific areas and how they connect back to the ROI attainment.

The ROI of IOT for OEMS - Reduce Time to Diagnose Field Issues - Parker Mobile IoTIn today’s day and age, one of the most crucial aspects of obtaining an exceptional customer experience is to make sure that you are valuing and prioritizing the customers’ time. Predictive service helps address this problem. By utilizing IoT to forecast when a piece of heavy equipment may need repairs or service, even under unexpected circumstances, OEMs can better manage and accurately schedule downtime on machinery and equipment, ultimately delivering a better service experience to customers. 

Better servicing not only leads to more satisfied customers, but it also provides operational gains. The benefit of an IoT solution for heavy equipment is that it helps the user better understand exactly what the problem is that needs to be examined from a remote location. This gives the technician a heads up and ensures they will have the right equipment, parts and skills to solve the issue and get things up and running again faster. 

Providing accurate updates to service technicians also smooths over the process of meeting compliance requirements for companies with service level agreements. The embedded IoT sensors not only help with the predictive servicing on machinery, but they also enable automatic reporting on asset health and communicate when thresholds have been reached. This feature dramatically improves the chances of meeting SLAs.

In addition to remote monitoring, predictive maintenance detects possible failures ahead of time, so an OEM can take corrective action at the right time to avoid unscheduled maintenance and unplanned downtime, thus mitigating project risks and reducing costs. For an OEM, predictive maintenance data is useful in terms of quality issues. An OEM can track historical failure data so corrective action can be put in place to avoid unnecessary downtime for additional customers due to unforeseen quality issue. 

The ROI of IoT for OEMs - Beyond Simple Tracking - Parker Mobile IoT

Combining, storing, and analyzing heavy equipment data is the kind of ‘deep learning’ required to take predictive maintenance to the next level. Data gathered on a piece of heavy machinery allows OEM to go from predicting when a known failure mode might occur to preventing it. This new learning is then incorporated to improve engineering knowledge that in turn helps build better models. Taking this to the next level, as we better understand failure modes and their predictors, and collecting even more precious data on a per machine basis, can enable OEMs to model performance for individual machines in terms of operator utilization and environmental impact. 

In addition to improving engineering and design concepts, OEMs can leverage data from an IoT solution for heavy equipment to create different types of equipment, with less simulation and modeling required. Using the real data from existing infrastructure, the options for finding new designs or even new uses for equipment can lead to new markets and new product lines for an OEM. This presents a massive opportunity for the OEM to ensure that they stay ahead of the competition.

OEMs realize that connected off-road equipment can help their customers reduce costs, increase productivity, and improve safety. These services not only add value for an OEM customer, they also increase brand loyalty, as other brands of equipment are not integrated with an existing IoT solution. Parker offers a customer-centric IoT solution, Mobile IoT, to meet the specific requirements of heavy equipment OEMs. As a result of implementing Parker’s Mobile IoT, OEMs are able to generate additional revenues not only from its data-driven offerings, but also from its core business through increased equipment sales and aftermarket services.
 

The ROI of IOT for OEMS - Financial Benefits Withing 2 Years - Parker Mobile IoTWhy partner with Parker?

For OEMs, building an IoT platform in-house can be costly as well as require years of development. Working directly with Parker enables OEMs to benefit from comprehensive technology integration and data analytics expertise to create valuable machine designs for customers without the cost or risk of building out a solution in-house. Click here to learn more about how Parker is positively impacting OEMs around the world from an IoT perspective. 

 

 

The ROI of IoT for OEMs Clint Quanstrom Motion Systems GroupArticle contributed by Clint Quanstrom, IoT general manager, and Kyri McDonough, marketing communications manager, Parker Hannifin Corporation.

 

 

 

 

Kyri McDonough, Group Marketing Communications Platform Lead, Motion Systems Group, Parker Hannifin

 

 

 

 

 

Other related topics on Parker Mobile IoT solution:

Parker Teams Deploying IoT to Help Customers Improve Operations
How IoT Systems Will Impact the Future for Off-Road Equipment
Modern Digital Ecosystems Take Mobile Hydraulic Systems to a New Level

The ROI of IoT for OEMs

Read more

Cold Weather Challenges Spur Design of New Low Temperature Hose cold weather equipment ParflexWhen it comes to hoses and cold weather performance, force to flex is not as important as actual hose construction. In harsh winter temperatures, hose construction materials can be a major contributor to hose failure. Over time, cold temperatures and UV rays dry out the core and jacket of a hose. This embrittlement of materials results in cracks. Cold sluggish fluid or low temperature fluids not compatible with the core materials can also add stress and cause damage.


Meeting the challenge

Parker engineers have been working closely with machine and vehicle designers for more than 30 years on the selection of optimal hoses. Cold Weather Challenges Spur Design of New Low Temperature Hose TOUGHJacket ParflexThe added stress of colder environments, led them to design the new, low-temperature hydraulic hoses which operate in temperatures as low as -70°F/-57°C with pressures operating up to 5,000 psi (345 bar). 


This new technology for low-temperature hydraulic systems has proven itself in a variety of different low and high-pressure applications, especially forklifts and aerial lift equipment or used in commercial freezers in harsh winter conditions. Applications range from low pressure fluid transfer, over-the-sheave, and steering lines to high-pressure hydraulics.


Designed for extended hose life

Parker low temperature thermoplastic hoses are built with a proprietary blend of materials specifically formulated to withstand repetitive flexing in cold temperatures. Cold Weather Challenges Spur Design of New Low Temperature Hose fork lift freezer application ParflexThe 563LT and 594LT offer the same abrasion resistance as Parker's standard hose but decrease component downtime in low temperatures. The ability of these hydraulic hoses to perform repetitive flexing in a cold environment opens a new range of possibilities for the industry while increasing product life. For the customer, excelling in cold climates means reduced change outs, reduced warranty maintenance and replacement costs.


Each hose is reinforced with either synthetic fibers, steel wire, or a layer of each, which enables assemblies to handle up to 5,000 psi (345 bar) working pressure (depending on hose selection). Available core tube options have a low coefficient of friction while maintaining excellent flexibility and a premier, abrasion resistant cover. This maximizes efficiencies and minimizes pressure losses to ensure long service life. 

Temperature deformation of the product does not affect the assembly’s chemical compatibility, technical performance or functionality. In addition, hose covers are durable and insensitive to UV or ozone exposure and thus, resistant to environmental stress.

 

ICUEE 2019 Conference

Attending ICUEE 2019? Visit us in Louisville, KY October 1 – 3 at booth #1826 to see the new hose. Not attending the show? Contact us for more information on low temperature thermoplastic hose.

 

Cold Weather Challenges Spur Design of New Low Temperature Hose Cedrick Barber Parflex DivisionThis article was contributed by Cedrick Barber, applications engineer, Parker Hannifin's Parflex Division

 

 

 

 

Related articles:

How Mobile Equipment Manufacturers Benefit from Using Formed Thermoplastic Hoses

Why Use Thermoplastic Hose?

What is Noise Generation in Hydraulic Systems?

 

Cold Weather Challenges Spur Design of New Low Temperature Hose

Read more

Latest Forum Posts