I need a copied parameters at one drive and transfer for other, but i select the install command the system apresents a error message that say " Network connections are not supported in DSElite, use the DSE" I need a install the DSE complete version or have a other solution for realize this process? I don't find the link to Dse Complete version Download, someone can help me a find?
The model of the drive is a AC890