Fluid purification is an essential task at hydroelectric dams. Water, entrained air and gases and solid particulates often contaminate turbine oil and hydraulic fluid and must be removed on a regular basis.
Conventional purifiers cannot start removing…
For optimum renewable energy performance, power generation equipment including transmissions, EHC drives, turbines, and transformers depend on clean hydraulic fluids and oil. When a hydraulic system becomes contaminated with air, water, or suspended solids…
Gearbox lubrication and thorough sealing of equipment in the Atlantis project.
The maritime industry is currently going through significant changes due to the introduction of tighter emission regulations. A stronger awareness in preserving the environment has pushed forward more stringent International Maritime Organization (IMO…
Today, ultra-pure water is a primary concern for operators of new and existing combined cycle power generation plants. Whether you are an EPC engineer designing a new power plant or an operations manager considering an equipment upgrade, partnering with…
Seals made of the fluoropolymer PTFE are used where many other sealing materials (such as rubber elastomers, polyurethanes, fabric-reinforced elastomer seals, etc.) reach their limits in terms of requirements such as temperature range, chemical, friction…
Ball valves are used in a variety of industries such as manufacturing, oil, and gas, automotive, marine, agricultural and heavy truck. Applications may vary but include operations for processing, transferring, pneumatic circuits, cooling, and measuring…
Industrial settings with strenuous applications, such as thermal cycling and vibration, are recognised as some of the toughest environments for tube fittings. In all cases such applications demand highly precise, leak-free technology to ensure protection…
Gas turbine performance is affected by the environmental challenges of a specific power plant installation. In a recent project located in the Middle East, a filtration solution to protect the turbine needed to be designed to address each of the conditions…
Industrial OEMs and end users rely on traditional tie-rod cylinders to deliver power to industrial presses, mills, foundries, power generation, oil and gas exploration and other extreme, heavy duty applications.
In today’s industrial manufacturing environment, hydraulic cylinders are complex devices that incorporate a wide range of components available in a multitude of sizes, configurations and materials. When it comes to complex hydraulic systems, cylinder…
Compressed air is one of the most critical and expensive utilities in any manufacturing facility. That said, maintenance and monitoring of this crucial system are largely ignored. When it is given attention, the focus is usually in the compressor room…