Food suppliers are always seeking ways to extend shelf life. Improved shelf life allows manufacturers to extend their geographical reach and allows the product to remain in stores and consumer's homes longer. Modified Atmosphere Packaging (MAP) is…
Twitter may be blocked in your country or by your firewall. Click here to visit the Twitter page.
Follow Parker Hannifin on social media:
Food suppliers are always seeking ways to extend shelf life. Improved shelf life allows manufacturers to extend their geographical reach and allows the product to remain in stores and consumer's homes longer. Modified Atmosphere Packaging (MAP) is…

For packaged wine to be successfully placed on the market within the country of import, it must be microbiologically stable, visually clear and particulate free.
The accepted method of achieving microbial stability is to filter the wine using membrane…
In today’s production environment, compressed air is widely used to automate processes, provide motive power, and package products. A clean, dry, reliable compressed air supply is essential to ensure manufacturing facilities maintain efficient and cost…
If your dust is combustible, you need to be concerned with the risk. According to a report published by Dust Safety Science¹, 34 dust explosions and 115 fires were logged globally in just the first six months of 2019. The incidents during this period resulted…
A tour of any modern manufacturing facility will uncover the extensive use of compressed air.
Production managers and quality managers may not be aware of the potential hazards associated with this common utility. Untreated, compressed air entering a…

Some of the world’s largest breweries have recently reported a decline in sales as they have admittedly failed to amend their brand portfolio to meet consumer trends. Sterile filtration could be the key to adapting to these changes to consumer…
Any trip to the supermarket will demonstrate just how popular healthy dairy products are – products which are low in fats, salts, sugars and preservatives. This trend has driven the growth of aseptic filling. However, the reduction in the use of preservatives…
As the craft beer sector continues to grow, mainstream beer sales continue to decline. Beer production in Europe has been in decline since the 1970s, and with more and more drinkers demanding a higher standard of drinks, the pressure for brewers to create…


Bacterial contamination in the dairy industry can have major implications for operators. It can result in product re-work, wastage or recall – the cost of which can run into millions of pounds once litigation, insurance pay-outs and reputational damage…

When it comes to the use of sterile gas for product contact purposes – such as aseptic packaging or product purge applications – no clear guidelines have been adopted by the dairy industry regarding the control of microbial hazards. Practices can often…
A question that is frequently asked when considering the installation of a nitrogen gas generator is "will the system create an oxygen-rich or oxygen-deficient atmosphere that could be potentially hazardous?"
Compressed air is used in a broad range of applications in the food processing industry. These applications include mixing of ingredients, cutting, sparging, drying of product, transporting and propelling food through processing systems, and packaging…
In many food processing and wet processing applications, the presence of moisture in electrical cabinets, motor housings and related equipment can lead to a variety of costly problems including premature component failure and poor product quality. In…
Snap open a bottle of beer and you will see, hear and feel the familiar fizz and bubbles. These sensations are the result of carbon dioxide (CO2), a colorless, odorless, non-combustible gas. While the main natural carbonation of beer occurs during the…
Many companies, including those in the food and beverage, pharmaceutical, cosmetics, manufacturing and electronics industries, recognize the negative effects on quality created by oil contact with their product during production. Product rejections and…
Since the advent of the semi-automatic water conditioning control valve followed by the automatic control valve, a common weakness has been the brine tubing connections between the brine valve and the brine tank. This circuit functions in two ways and…
Our sense of taste is changing. We’re becoming more health conscious of the foods and beverages we consume to living a better life. No more perplexing and hard-to-pronounce food labels. Rather, simplicity rules the day as consumers seek transparency in…
Using a variable frequency drive (VFD) can be beneficial in many constant speed applications driven by electric motors, such as those that require controlled starting and have been historically served by a reduced voltage soft-starter (RVSS). While an…
Many companies, including those in the food and beverage, pharmaceutical, cosmetics, manufacturing and electronics industries, recognize the negative effects on quality created by oil contact with their product during production. Product rejections and…