The performance of gas turbines (GT) for power generation has a fundamental influence on the bottom line. Lack of availability, reduced power output and maintenance overheads all link directly back to profitability. As the efficiency of GTs continues to…
The increased reliance on renewable forms of energy makes it more important than ever to identify energy sources that can efficiently supplement the variable output and available peak load capacities of such renewable sources like wind and solar power…
Although wind currently provides 5 percent of the world’s electricity, the growing push for renewables has led many scientists and engineers to predict that wind turbines may generate at least half of all power by 2050. That is not a given, however, as…
The global gas turbine market is expected to experience substantial growth in both the short- and long-term in response to a growing need for a reliable, cost-effective electric supply with few carbon emissions. Such growth is being spurred by increased…
As regulatory pressure continues to curb greenhouse emissions, there has been a lot of attention on solar and wind energy. However, a less-publicized renewable energy source could play a major role in preparing for a world that is less dependent on fossil…
As renewable energy sources such as wind and solar become a larger part of the overall United States’ energy portfolio, energy producers and system operators have an opportunity to take advantage of expanding options to introduce renewable energy to the…
Biogas is a renewable energy source that can be used to generate heat and electricity. It’s produced through the decomposition of organic materials from plants and animals, also known as “biomass.” Further refined through a renewable natural gas production…
The potential for wind energy is massive. Although wind energy currently represents only about five percent of the world’s total electricity, many experts predict it could easily produce at least one-fourth to one-third of the world’s total production…
During the past 60 years, the use of the natural gas combined cycle (NGCC) process for electricity generation has grown to make it one of the world’s leading sources of power. Along the way, natural gas combined cycle efficiency has improved because of…
For decades, coal has dominated global power generation. Yet, its share of power generation is declining. The International Energy Agency predicts that global coal consumption has peaked and will not return to former levels, as cited in an article appearing…
The sun has been referred to as a primary inexhaustible energy source capable of meeting energy demands on a global scale. Electricity can be generated from solar energy either directly using photovoltaic (PV) cells or indirectly using concentrated solar…
In baseball, a utility infielder is a reliable and versatile player who can fill in at multiple positions depending on the needs of the team. In 21st-century power generation, a reciprocating engine can play such a role.
Increasing customer demand requires new process applications with needs for reliable lubrication and resistance to galling under stringent conditions of temperature, pressure, vacuum, corrosive environments, process sensitivity to contamination, product…
In a Concentrating Solar Power (CSP) system, solar radiation is collected and concentrated, multiplying the sun's ambient heat to temperatures in excess of 750°F. In the most common application of CSP today, this is accomplished through parabolic…
Wind turbines are designed to maximize power production based on the predicted wind speeds found at the plant site. However, excessive wind speeds are experienced at times, so it is crucial to limit power generation at those times to avoid spontaneous…
Power generation plants rely heavily on demineralized and deionized water to maintain required levels of water purity during process operations. Managing the water supply is critical under normal operating conditions, as well during outages. The introduction…
For power plants located in moisture-rich environments, such as coastal locations, high levels of humidity, rain, fog, mist and sand can damage and impair the performance of the gas turbine. Coalescers are installed to remove moisture and liquid phase…
Wind power generation in the U.S. has been trending favorably upwards for wind farm owners. Primary contributing factors include the cost of wind turbine installations dropping by over one-third since 2010 as the capacity of turbines increased. Add-i…
The maritime industry is currently going through significant changes due to the introduction of tighter emission regulations. A stronger awareness in preserving the environment has pushed forward more stringent International Maritime Organization (IMO…
Industrial OEMs and end users rely on traditional tie-rod cylinders to deliver power to industrial presses, mills, foundries, power generation, oil and gas exploration and other extreme, heavy duty applications.
In today’s industrial manufacturing environment, hydraulic cylinders are complex devices that incorporate a wide range of components available in a multitude of sizes, configurations and materials. When it comes to complex hydraulic systems, cylinder…