There are many types of bearing greases for aviation wheel assemblies. Here, we will examine the four main types of bearing grease used by Parker's Aircraft Wheel & Brake Division, an industry leader in the design, manufacture, and support of superior braking systems since its founding in 1936.
Safety is the first step
1. Be sure to always use eye protection and rubber gloves when cleaning repacking or handling bearings.
2. Also remember to never mix any two bearing greases together because it may result in premature failure of the bearing.
3. Always replace bearings as a set cup and cone.
Types of greases
The four types of bearing greases used by Parker Aircraft Wheel & Brake Division are:
- SHC 100 Mobil aviation grease
- Aeroshell grease 22
- HCF grease P/N 605 (amphibious)
- OMNIi waterproof grease number 2 (amphibious)
Cleveland Wheel and Brake technicians and service guides and general maintenance manual calls out to specifications mill PRF81322 and D O D G245088.
SHC 100 Mobil aviation grease
The first of the four greases we will explore is SHC 100 Mobil aviation grease. This grease is synthetic and provides a high dropping point. It has excellent resistance to water wash, and it is an outstanding protector against wear corrosion and high temperature, which can be damaging. And finally, it is red in color.
Aeroshell grease 22
The Aeroshell grease 22 is a versatile multi-purpose grease for aircraft wheel bearings. It is recommended for general anti-friction bearings operating at high speed and at high or low temperatures, this grease is brown in color.
HCF grease P/N 605 (amphibious)
The HCF grease P/N 605 is an amphibious grease. It provides protection against the corrosive action of fresh water, salt, water, and chemical fumes. It maintains lubricating film under adverse conditions of load and torque, and it is dark brown in color.
OMNI waterproof grease number 2 (amphibious)
The fourth grease is the OMNI waterproof grease number two, which is also an amphibious grease. This grease acts as a rust preventative protecting bearings seals and open gears against costly wear. It repels fresh or salt waters. This grease is green in color.
Now, watch the training video
For more information on greases and other topics like this, please visit our website.
This blog was contributed by the Aerospace Technology Team, Parker Wheel & Brake Division.
Related content
Defining Our Unique Contribution to the World
Eighty Years of Innovation at Parker Aircraft Wheel & Brake
Partnership with Piaggio Results in Reduced Maintenance Costs
Aerospace Technologies and Key Markets
For decades, futurists have been dreaming of “flying cars” that are easier and nimbler to operate than a helicopter and accessible to everyone. Today, many aerospace technologies are coming together helping numerous companies develop small passenger electric aircraft as soon as 2023.
According to a 2020
More-electric aircraft
Cockpit controls – Parker Aerospace
Electro-mechanical actuators
Electric motors and controllers
Advanced thermal management solutions
Vibration attenuation and motion control
As a trusted partner, Parker's team members work alongside customers to enable technology breakthroughs that change the world for the better. We help our customers and distribution partners meet the newest standards for safety or emissions, reduce power usage, improve efficiency, and move faster to optimize resources.
This blog was contributed by Chris Frazer key account manager and UAM/eVTOL/AAM business development lead of Parker Aerospace.
The future of air travel is evolving beyond fossil fuels with hybrid electric and all-electric aircraft leading the way. The growing need for low emissions and carbon neutrality has created a new focus on more electric aircraft (MEA), as aircraft original equipment manufacturers (OEMs) look to satisfy the growing needs of travelers while achieving the environmental goals being mandated around the world.

An individual SSPC can be programmed and coordinated with other SSPCs to provide staggered power on/off configurations when used in a multi-channel configuration. Power sequencing, source and load isolation, power routing, and bi-directional flow for battery charge/discharge, can all be configured in the same SSEDU. Voltage, current, temperature and other performance and fault data is available for each SSPC.
Current development on the second-generation SSPC will culminate with a two-channel unit in a more compact, thermally efficient, and lighter unit. This fully capable demonstrator will provide an example of how the Parker Aerospace SSPC and SSEDU can be utilized for multiple applications and configurations requiring the control, protection, and flexibility required to satisfy the needs of the new generation of more electric aircraft.
This blog was contributed by electronics engineering manager Andrew Walsh from the
When people think of the
An idle aircraft is an expensive and complex reality for airlines trying to serve thousands of people. When such an event occurs, the EMFAS team delivers on its mission to serve airline customers and keep their fleet of aircrafts doing what they are designed to do: move people and goods as seamlessly and safely as possible.
EMFAS team members work in a dynamic environment. Every day brings new adventures, issues, customers, and people. These technical experts find it rewarding to help customers solve problems, develop relationships, and work with people from nearly every continent.
Most service businesses are built on relationships. Customers consider a company only as good as its last order. EMFAS views itself as a service business rather than a company that manufactures a product. There are no long-term contracts and no ownership of the intellectual property on the parts they repair so they must perform at the highest level every time.
Since 2002, the EMFAS team has had an excellent performance track record with customers. In the first year of operation, EMFAS had five customers; today it has more than 250. EMFAS is a successful team that supports partners internally and externally. With the full support of Parker, EMFAS is just getting started, and the brightest times are ahead.
This blog was contributed by Chris Capuano of