Electromechanical Group

Electromechanical is the technology of controlling mechanical devices via electricity. Parker electromechanical systems and components improve precision and increase productivity.
Electromechanical Knowledge Base
Group - List
Latest Electromechanical and Drives Blog Posts

Variable Speed Drives Car Park Parker Hannifin EMDEThe renewal of the entire ventilation system in the underground car park serving the largest European business district, was not limited to the simple replacement of filters and some mechanical components. This operation involved a vast project requiring advanced technical expertise, particularly in terms of defining and selecting drive solutions and supporting their integration, installation and commissioning.

The objective of the drive systems for the variation of ventilation speed was two-fold. Firstly, it was a question of ensuring the effective evacuation of exhaust gases. Then, secondly, achieving much faster removal of smoke in the event of a fire. The previously installed system had become obsolete because it was only equipped with two-speed motors without drives.


Variable Speed Drives Car Park Parker Hannifin EMDEParker worked with EDF and Inov Industrie on the project. The company was selected for its technical abilities with respect to drive systems, but perhaps more importantly, for its "know how" in the control of energy consumption/optimisation of energy efficiency. The project presented multiple challenges that had to be overcome. First, the project concerned the most extensive car park in Europe incorporating 22,000 spaces, spread over sixteen different sites. Then, due to the underground location of the car parks, below the towers of La Defense at a complex, major road junction, there were numerous access constraints. To this was added the problem of dimensions: the systems selected had to fit in existing cabinets and be adapted to the protocol already in place.

 

Enhanced performances at your fingertips

All of the disassembled components being replaced had to be removed and recycled. Finally, and perhaps most importantly, the fire safety system needed to allow the forced operation of the drives at maximum speed in order to reliably evacuate fumes in the shortest possible time. For safety, the new systems also needed to be equipped with an automatic restart and be directly connected to the emergency fire services.

The nature of the project meant that work had to be completed quickly and efficiently under intense time pressure. The scale of the project meant that a total of 60 drives with power ratings from 5.5kW to 180kW had to be commissioned in a very short space of time. Inov Industrie, with its 20-year working relationship with Parker, turned to the motion and control specialist, opting to specify units from the company’s AC10 compact drive range.

 

Variable Speed Drives AC10 Series Parker Hannifin EMDESimple and reliable motor control

The suitability of the AC10 range for this significant and challenging project was enhanced due to some new features such as fire mode input/output and its wide range of power ratings - all in a compact package. The AC10 range is characterised by its simplicity of installation, setup, and commissioning, thanks in particular to a fast parameterization. With its enhanced functionality, the AC10 drive is able to control asynchronous motors incorporating both simple and complex types of application such as pressure and flow control. The ‘small sequential’ function (sequencing on and off) avoids the need for an additional PLC. It is also possible to obtain information relating to system power consumption and other parameters such as the occurrence of dirty filters.

 

Francis Scharwatt Parker Hannifin FranceArticle contributed by Francis Scharwatt, sales engineer, Parker Hannifin France

 

 

 

 

 

Related content:

How Variable Speed Drives Become Simpler and More Efficient

Inverters Help Make the Most of Green Energy

VFD Eliminates Bottleneck in Canning Plant

Meeting Demand for Efficient Automotive Vehicle Testing & Dynamometers

Improve Safety and Air Quality in Europe’s Largest Underground Car Park

Read More

Variable Speed Drives Car Park Parker Hannifin EMDEThe renewal of the entire ventilation system in the underground car park serving the largest European business district, was not limited to the simple replacement of filters and some mechanical components. This operation involved a vast project requiring advanced technical expertise, particularly in terms of defining and selecting drive solutions and supporting their integration, installation and commissioning.

The objective of the drive systems for the variation of ventilation speed was two-fold. Firstly, it was a question of ensuring the effective evacuation of exhaust gases. Then, secondly, achieving much faster removal of smoke in the event of a fire. The previously installed system had become obsolete because it was only equipped with two-speed motors without drives.


Variable Speed Drives Car Park Parker Hannifin EMDEParker worked with EDF and Inov Industrie on the project. The company was selected for its technical abilities with respect to drive systems, but perhaps more importantly, for its "know how" in the control of energy consumption/optimisation of energy efficiency. The project presented multiple challenges that had to be overcome. First, the project concerned the most extensive car park in Europe incorporating 22,000 spaces, spread over sixteen different sites. Then, due to the underground location of the car parks, below the towers of La Defense at a complex, major road junction, there were numerous access constraints. To this was added the problem of dimensions: the systems selected had to fit in existing cabinets and be adapted to the protocol already in place.

 

Enhanced performances at your fingertips

All of the disassembled components being replaced had to be removed and recycled. Finally, and perhaps most importantly, the fire safety system needed to allow the forced operation of the drives at maximum speed in order to reliably evacuate fumes in the shortest possible time. For safety, the new systems also needed to be equipped with an automatic restart and be directly connected to the emergency fire services.

The nature of the project meant that work had to be completed quickly and efficiently under intense time pressure. The scale of the project meant that a total of 60 drives with power ratings from 5.5kW to 180kW had to be commissioned in a very short space of time. Inov Industrie, with its 20-year working relationship with Parker, turned to the motion and control specialist, opting to specify units from the company’s AC10 compact drive range.

 

Variable Speed Drives AC10 Series Parker Hannifin EMDESimple and reliable motor control

The suitability of the AC10 range for this significant and challenging project was enhanced due to some new features such as fire mode input/output and its wide range of power ratings - all in a compact package. The AC10 range is characterised by its simplicity of installation, setup and commissioning, thanks in particular to a fast parameterization. With its enhanced functionality, the AC10 drive is able to control asynchronous motors incorporating both simple and complex types of application such as pressure and flow control. The ‘small sequential’ function (sequencing on and off) avoids the need for an additional PLC. It is also possible to obtain information relating to system power consumption and other parameters such as the occurrence of dirty filters.

Francis Scharwatt Parker Hannifin FranceArticle contributed by Francis Scharwatt, sales engineer, Parker Hannifin France

 

 

 

 

 

Related content:

How Variable Speed Drives Become Simpler and More Efficient

Inverters Help Make the Most of Green Energy

VFD Eliminates Bottleneck in Canning Plant

Improve Safety and Air Quality in Europe’s Largest Underground Car Park

Read More

1Maintaining a safe and productive work environment should be top priority in any facility. More and more companies are putting programs in place to improve the working environment and thereby increase the performance of workers.

Audible noise is one of the factors most commonly present on the manufacturing floor, since the operation of any equipment or machinery involves the generation of noise at some level. Usually, the lower the technology of the equipment, the greater the intensity of the noise emitted, reaching in some cases to exceed the tolerable or legally allowed levels.

In addition to the risk of hearing loss, excessive noise has been known to cause physiological effects such as fatigue, tinnitus, lack of concentration and stress, even at levels well below 85 decibels (dB). Keeping people working in environments with excessive noise is a safe bet for reduced productivity and lost time.

Corrective actions for noise control

Excessive noise exposure can be mitigated by addressing several elements. The actions for noise control can be classified according to the element on which they are carried out:

  • Noise generation source (machine or equipment)
  • Means of propagation
  • Receiver (worker)

Directly reducing the noise generated by the source is the ideal option because it eliminates the need to add elements external to the process and results in a more efficient operation, but can potentially require more initial investment. Among the actions of this type we find:

  • Update to more modern technologies
  • Major maintenance of the machinery

When it is not possible to act on the noise source, or the reduction reached is not enough, it is possible to alter the propagation medium to reduce the sound effect. These actions have the advantage of being able to be carried out without modifications to the production process, representing a fairly low implementation risk. Among these actions we have:

  • Cabinets or enclosures for the machine
  • Anti-vibration mounts to avoid resonances

The noise control actions in the receiver must be the last ones due to the inconvenience that it generates for the worker and the consequential reduction of the effectiveness of oral communication. These actions are typically:

  • Ear protector like plugs and shells
  • Enclosure booths for workers
2Noise reduction cabinets with Parker IPS

Parker's t-slot aluminum profile system (IPS) is an excellent solution for the manufacturing of enclosure cabinets and noise reduction barriers. The flexibility of the system allows adaptation of the design to the specific geometry of the machine and provides semi-fixed sections that facilitate access for operation and maintenance.

The wide selection of panels allows to have opaque or transparent walls and profiles with double grooves allow the easy fabrication of walls with double panels that increase the attenuation of the noise.

Parker IPS profiles are easy to modify and totally reusable, so you will not only be satisfying your current needs but also future ones. A great way to get started on a Parker IPS project is to download our T-slot Aluminum Design Architect software and start designing today. 

To learn more: Visit our website.

1

Article contributed by Julio Sanchez, IPS product manager, Parker Mexico. 

 

 

 

Related Content:

Choosing Between Steel or Aluminum Structural Framing

Putting It All Together: Choosing a Fastening Method

A Quieter Approach to Laboratory Equipment Design

Solutions for Reducing Noise on the Factory Floor

Read More

Key Technology Considerations for Dynamic Metrology Applications Electromechanical DivisionThroughout the world various types of metrology applications share a common need for increased precision. Metrology is the scientific study of measurement. Metrology applications take some type of measurement to collect certain data. Markets such as life science, semiconductor and electronics manufacturing rely on metrology instrumentation to ensure their process is completed correctly. The need for precision is further underscored when you realize the samples/products can be extremely small (i.e. human cell) as well as highly sensitive (i.e. touch-screen electronics). Having high precision motion technology is key to ensure the application will be completed successfully. 

This blog post will cover the basics of metrology applications, but if you are interested in learning more, Parker has published a detailed white paper on the topic, which we encourage you to download here

Metrology applications

Listed below are some examples of metrology applications by market. Many applications can be used in more than one market as well. For example, all the markets will use some type of microscopy in their process.

Life science  

  • Microscopy
  • Spectroscopy
  • DNA sequencing

Semiconductor

  • Wafer inspection
  • Lithography
  • Optical profilometry

Electronics

  • Laser profilometry
  • Non-contact metrology
Types of metrology applications

There are different types of metrology applications, and each have their own key considerations. This blog post will focus on dynamic metrology.

  • Dynamic metrology – applications where measurement data is collected while either the measurement sensor or the unit under measurement are in motion
  • Static metrology – applications where measurement data is collected while both the measurement sensor and the unit under measurement are at a stable location
  • Focusing – a special type of static metrology where an axis, typically vertical, is used to focus on a sample for measurement
Dynamic metrology
Static metrology requires good velocity and profile control, while dynamic applications require settling and stability control. Dynamic metrology applications are more and more commonly associated with laser-based, spectrometry and applications in the high-tech markets. Semiconductor and electronics manufacturing use line scanning at some point in almost all their processes, while life science instrumentation performing high content throughput cell analysis or DNA/gene sequencing is also dynamic. Precision laser cutting is also a dynamic application. Since the actuator is in motion while measurements are being taken, the critical specifications relate to its motion performance, including:
 
  • Errors in positioning are normally specified in terms of the accuracy of positioning and the repeatability of positioning. The actual sources of these errors can occur in three sub categories – linear, Abbe (roll, pitch, yaw) and planar errors. The source for these errors varies and could have occurred during production or while the application is in process. Examples include deflection, friction, bearing and machining inconsistencies and feedback device.

Yaw Pitch and RollFlatness and Straightness

  • Velocity control relates to the speed of the stage’s motion and the ability to control it. When there is a variation of velocity as compared to the commanded velocity, this is known as a velocity ripple. Velocity control is critical for dynamic metrology applications because if the speed varies throughout the application process, accurate and consistent results will not be obtained throughout.

                                                        Settling Time

The best actuator option for dynamic metrology applications requiring high precision and speed is a linear motor driven stage, specifically one with an ironless linear motor. Since the linear motor couples directly to the linear load, backlash, efficiency losses and other positional inaccuracies are greatly reduced compared to screw or belt driven actuators. Also, linear motors typically have a smaller form factor which overall will improve the stiffness and positional errors. Finally, linear motor actuators have the best control of its speed throughout the application. 

While maintaining a reasonable commercial cost, linear motor actuators are the only ones that can meet the critical specifications for dynamic metrology applications previously discussed. To confirm this, Parker uses a laser interferometer to measure any potential positional errors. After testing, reports on the actuator’s performance are generated which consistently show that linear motor actuators outperform those with other drive train mechanisms. 

Further details on dynamic metrology download the whitepaper, "Understanding Critical Specifications for Dynamic Metrology Applications." 

Parker metrology application solutions

Stage stability and velocity control on a linear motor actuator are crucial in order to have a successful dynamic metrology application. With over 20 years of experience in the high technology precision markets, Parker offers the expertise and consulting services to help instrumentation developers optimize the precision of their equipment and their process. These process optimizations will contribute to continued reductions in the customer’s overall spend, while throughput increases. You can learn more about Parker’s linear motor stage capabilities by visiting our website.

Patrick Lehr

Article contributed by Patrick Lehr, product manager for precision mechanics, Electromechanical and Drives Division North America, Parker Hannifin Corporation. 

 

 

 

 

Related content:

Practical Applications for Precision Electromechanics in Photonics

How to Specify Precision Linear Mechanics for a Cleanroom Environment

Seven Factors to Consider When Selecting Linear Mechanics for a Vacuum Environment

Key Technology Considerations for Dynamic Metrology Applications

Read More

Test Rigw with Parker High Speed Motor MGV When it comes to gearbox test rigs deployed in the automotive and aerospace industries, one thing is certain - there is no margin for failure. A test rig or system that is unreliable or produces erroneous results can have serious consequences to development programmes where designers and research and development engineers are under intense pressure to deliver next-generation solutions to a demanding customer base.

Gearbox test rigs come in many different configurations, depending on the type of transmission being tested. However, most share a common requirement, namely the need for electromechanical components such as high-speed servomotors, inverters and linear motors.

A case in point can be seen at BIA, a French-based industry leader in the design, development and manufacture of test equipment and systems for customers in the aerospace, industrial and automotive sectors. The company has been collaborating with specialists at Parker for a number of years, with the outcome that BIA is now able to combine specific elements and components of its test rigs into completely bespoke, integrated systems that offer higher reliability and performance.

Gearbox Test Rigs Need Reliable, High-Precision Parts - BIA Olivier Carlier

We very much benefit from Parker’s wide product offering that helps us to efficiently source high quality and reliability components and systems, which finally contribute to BIA’s global success. We appreciate the very constructive spirit with which the dialogue with Parker is conducted." 

Olivier Carlier. project leader at BIA

 

 

 

Parker works closely with customers such as BIA to help define the components required for each individual simulation and test system. Here, the company’s extensive portfolio assists in sourcing high quality, reliable products and systems. Products such as Parker’s high-speed servomotors, for example, are adopted widely in gearbox test rigs for the efficiency of their cooling systems, as are Parker linear motors, chiefly as a result of their positioning accuracy.

 

High Speed Servo Motor for Test RigsBeginning with Parker’s brushless, permanent-magnet, high-speed MGV servomotors, these offer the capability to simulate a combustion engine in conjunction with a vehicle’s manual gearbox. Of particular note, MGV motors benefit from water cooling, which in turn permits their dimensions and operating noise to be minimised. Furthermore, the low inertia of the MGV allows for highly dynamic acceleration and deceleration, while in order to achieve maximum precision, motor speed and torque are controlled in a closed loop, permitting the servomotor to be used for simulations in both urban traffic and race conditions.

Parker MS asynchronous motor are also popular for gearbox testing applications. The reason stems from the fact that the MS can deliver 10,000 rpm at 500 kW, which is ideal for gearbox duration testing – a task which requires a constant, medium speed without acceleration.

On the subject of transmission endurance tests, Parker ETT linear motors are often deployed (including at BIA) to actuate the gear lever and engage gears. Here, the rectangular rod configuration connected to ETT cylinders simulates movement through the standard H-slots of the gear lever. ETT linear motors have a high positioning accuracy of 0.5 mm, along with repeatability of 0.05 mm. 

Also worthy of mention, Parker AC890 inverters have been developed to achieve optimum performance levels with both asynchronous motors (MS) and synchronous servomotors (MGV), and are able to operate in both motor and generator modes. This functionality can be exploited during gearbox tests: one motor can be connected to the gearbox input, just like a diesel engine, while two other motors (operating in generator mode) can be linked with the output of the gearboxes to simulate rotating wheels. This power generation gives full grid energy recuperation and can enable significant energy savings too.

 

M.Finck Article contributed by Michel Finck, market development manager, Electromechanical & Drives Division Europe.

 

 

 

 

 

Related content:

Meeting Demand for Efficient Automotive Vehicle Testing & Dynamometers

A Simple Guide to Benefits of Electromechanical Technology

Electromechanical Technologies and Key Markets

 

Gearbox Test Rigs Need Reliable, High-Precision Parts

Read More

Test Rigw with Parker High Speed Motor MGV When it comes to gearbox test rigs deployed in the automotive and aerospace industries, one thing is certain - there is no margin for failure. A test rig or system that is unreliable or produces erroneous results can have serious consequences to development programmes where designers and research and development engineers are under intense pressure to deliver next-generation solutions to a demanding customer base.

Gearbox test rigs come in many different configurations, depending on the type of transmission being tested. However, most share a common requirement, namely the need for electromechanical components such as high-speed servomotors, inverters and linear motors.

A case in point can be seen at BIA, a French-based industry leader in the design, development and manufacture of test equipment and systems for customers in the aerospace, industrial and automotive sectors. The company has been collaborating with specialists at Parker for a number of years, with the outcome that BIA is now able to combine specific elements and components of its test rigs into completely bespoke, integrated systems that offer higher reliability and performance.

BIA Olivier CarlierWe very much benefit from Parker’s wide product offering that helps us to efficiently source high quality and reliability components and systems, which finally contribute to BIA’s global success. We appreciate the very constructive spirit with which the dialogue with Parker is conducted."  Said OLIVIER CARLIER. Project Leader at BIA

Parker works closely with customers such as BIA to help define the components required for each individual simulation and test system. Here, the company’s extensive portfolio assists in sourcing high quality, reliable products and systems. Products such as Parker’s high-speed servomotors, for example, are adopted widely in gearbox test rigs for the efficiency of their cooling systems, as are Parker linear motors, chiefly as a result of their positioning accuracy.

High Speed Servo Motor for Test RigsBeginning with Parker’s brushless, permanent-magnet, high-speed MGV servomotors, these offer the capability to simulate a combustion engine in conjunction with a vehicle’s manual gearbox. Of particular note, MGV motors benefit from water cooling, which in turn permits their dimensions and operating noise to be minimised. Furthermore, the low inertia of the MGV allows for highly dynamic acceleration and deceleration, while in order to achieve maximum precision, motor speed and torque are controlled in a closed loop, permitting the servomotor to be used for simulations in both urban traffic and race conditions.

Parker MS asynchronous motor are also popular for gearbox testing applications. The reason stems from the fact that the MS can deliver 10,000 rpm at 500 kW, which is ideal for gearbox duration testing – a task which requires a constant, medium speed without acceleration.

On the subject of transmission endurance tests, Parker ETT linear motors are often deployed (including at BIA) to actuate the gear lever and engage gears. Here, the rectangular rod configuration connected to ETT cylinders simulates movement through the standard H-slots of the gear lever. ETT linear motors have a high positioning accuracy of 0.5 mm, along with repeatability of 0.05 mm. 

Also worthy of mention, Parker AC890 inverters have been developed to achieve optimum performance levels with both asynchronous motors (MS) and synchronous servomotors (MGV), and are able to operate in both motor and generator modes. This functionality can be exploited during gearbox tests: one motor can be connected to the gearbox input, just like a diesel engine, while two other motors (operating in generator mode) can be linked with the output of the gearboxes to simulate rotating wheels. This power generation gives full grid energy recuperation and can enable significant energy savings too.

 

M.Finck Article contributed by Michel Finck, market development manager, Electromechanical & Drives Division Europe.

 

 

 

 

 

Related content:

Meeting Demand for Efficient Automotive Vehicle Testing & Dynamometers

A Simple Guide to Benefits of Electromechanical Technology

Electromechanical Technologies and Key Markets

 

Gearbox Test Rigs Need Reliable, High-Precision Parts

Read More

Latest Electromechanical and Drives Forum Threads