Hello!
DC Drive 590+ Frame 3 max.armature current 270A
I have the potentiometer for the regulating speed!
Potentiometer connected to B3 +10V and A1 0V And to terminal A4 for the regulating!
Can i use the external +10 volts for the speed regulating?
I want take off the potentiometer and connect external +10 volts from the Scneider PLC Analog card!
I need regulate speed from the PLC
How can i make it better?
Best regards,
Dmitri