When the unit boots up I see the following sequence:
c:\CTC>biostr
Load Hardware-Specific Functions EX-82524-200
Display type not recognized!
Initialization Failure...exiting.
Then the unit continues to boot, communicates with the PLC properly and all visual functionality works as expected but the pointer for the touchscreen doesn't appear to be calibrated properly. I'm unable to touch any of my pushbuttons or get it to respond. I've tried to hook up a keyboard, exit to the shell and calibrate the touchscreen but that option is grayed out. Is there any way to resolve this Display Type problem?
Thanks.