Hi,
I previously posted for help on this drive regarding error code 3, which unfortunately cannot be resolved. Link... https://community.parker.com/technologies/electromechanical-group/f/support/471/digiplan-blx75b-showing-error-code-3---eprom-memory-map-changed-but-unable-to-clear-fault/937#937
I'm now looking to purchase a second hand drive and copy the parameters from a known good drive to it but there seems to be no way of doing this.
Using the XU command I have verified that there are no stored sequences in the drive. But there seems to be no equivalent for drive parameters?
Does anyone know of a command for the upload of all parameters, to the terminal I presume?
And also downloading parameters, or is this done manually(!) ?
Kind regards,
Matt