I'm using a Parker 514C SSD to control my DC motor and need to know how much current the control terminals T14 & T16 can safely handle. These are the +-10V reference outputs used to power the speed potentiometer for motor speed control.
The manual says they are 5mA output but I need to use the 650 Ohm rheostat currently in the machine for motor speed control and that puts me at about 15mA. Is there head room on these terminals to safely handle the increased current draw?