i have PSD servo drive without power module and connect 24VDC on terminal and i try to connect it with pc through ethernet cable and gives (failed to connect to PSD and gives no ping response)
i have PSD servo drive without power module and connect 24VDC on terminal and i try to connect it with pc through ethernet cable and gives (failed to connect to PSD and gives no ping response)
What is the part number of the PSD? There are many different configurations of the PSD line.
Also when the PSD is powered on, what is the status of the LEDs.
Also make sure that you are connecting the ethernet cable to x60 port which is the closest ethernet port to the front of the PSD. And the ethernet cable needs to be a cross-over cable and not a patch cable.
The IP address of you PC's ethernet adapter needs to be 192.168.10.xx where the xx is something other than what is set up for the PSD and is calculated from S12 and S13. More information on this can be found on page 38-39 in the PSD Installation Guide.