i have PSD servo drive without power module and connect 24VDC on terminal and i try to connect it with pc through ethernet cable and gives (failed to connect to PSD and gives no ping response)
i have PSD servo drive without power module and connect 24VDC on terminal and i try to connect it with pc through ethernet cable and gives (failed to connect to PSD and gives no ping response)
What is the part number of the PSD? There are many different configurations of the PSD line.
Also when the PSD is powered on, what is the status of the LEDs.
Also make sure that you are connecting the ethernet cable to x60 port which is the closest ethernet port to the front of the PSD. And the ethernet cable needs to be a cross-over cable and not a patch cable.
The IP address of you PC's ethernet adapter needs to be 192.168.10.xx where the xx is something other than what is set up for the PSD and is calculated from S12 and S13. More information on this can be found on page 38-39 in the PSD Installation Guide.
concerning setting IP address I adjust it correctly But when we enter network sharing i find ethernet connection is unpluged (lamps yellow or green for ethernet is turned off)
Please clarify. Are you saying P13 and P14 are coming on, but your Ethernet lights are not? If so, then that means you have successfully applied power to the drive. That is all you should need to do to get the Ethernet lights to work. If the Ethernet lights still do not come on, you might have a bad Ethernet cable. You might also have a bad Ethernet port on your PC or on the PSD.
Complete wiring information for the PSD can be found in the manual here: 192-011006N8 PSD1 Installation Guide (parker.com)
Please clarify. Are you saying P13 and P14 are coming on, but your Ethernet lights are not? If so, then that means you have successfully applied power to the drive. That is all you should need to do to get the Ethernet lights to work. If the Ethernet lights still do not come on, you might have a bad Ethernet cable. You might also have a bad Ethernet port on your PC or on the PSD.
Complete wiring information for the PSD can be found in the manual here: 192-011006N8 PSD1 Installation Guide (parker.com)