Print Friendly and PDF

690 control board on 890 chassis.

Is it still possible to use 690 control board on a 890 chassis? In the past (15 years ago) the 690 chassis and 890 chassis were exactly the same (above 30kW). This would be useful since 690 has become obsolete. Maybe it will not work anymore because of STO function on 890 chassis?