Hello everyone,
I have a shredder with 2x 4Kw Siemens motors and gearboxes that makes 6100Nm of torque for each axle with those motors.
I received the shredder 3 days ago and installed it yesterday, but it does not perform as expected.
Ive tried to shred a car tire, and it does not do that.
So i guess there is something wrong with the settings on AC10 unit.
F801 is at 8 and F803 is set at 16.4
At this moment i have both motors hooked up to the VFD because im still waiting for a second AC10 to arrive.
Could this be the problem?
My knowledge is very limited on the VFD so all help is welcome !
Thanks in advance !