Print Friendly and PDF

Word (Other than Comms control word, comms reference word) transfer between S7-300 & AC30 over profibus

I need to send a Word (other than comms control word & comms reference word) from my S7-300 PLC to AC30 drive over profibus & then use it bit by bit in PDQ. Which parameter should I select in Read mapping? Similarly, I need to convert a set of bits to Word in PDQ and then send it to the PLC. Which parameter should be linked to write mapping.