Print Friendly and PDF

Analog disconnected protection in AC10 FW3.32 does not work

Hello,

Parker AC10, FW3.32 feature Analog disconnected protection (F741=1) does not work at all.

I confirm that this feature is working as described in the user manual in FW2.31.

Can you please suggest workaround.

Regards,

Parents
  • Hello Dusan,

    The AC10 frame sizes are major firmware dependent. If it was working fine in 2.31, please revert back to a v2.x version of firmware as you probably have a Frame1-5 drive correct? The latest version of firmware for v2.x units, is v2.33.

    From DSELite for illustration, below. V2.x is for frames 1-5. V3.x is for frames 6-12.  v4.x is for the IP66 drives.

        

Reply
  • Hello Dusan,

    The AC10 frame sizes are major firmware dependent. If it was working fine in 2.31, please revert back to a v2.x version of firmware as you probably have a Frame1-5 drive correct? The latest version of firmware for v2.x units, is v2.33.

    From DSELite for illustration, below. V2.x is for frames 1-5. V3.x is for frames 6-12.  v4.x is for the IP66 drives.

        

Children