Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Configure a TCP/IP Dial-Up Adapter Connection.
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Configure a TCP/IP Dial-Up Adapter Connection.
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)-
      • Replace/Upgrade Interact panel P11/P1H/P15/P2/P3/P4/P5 etc
      • CTC and i-Motors
      • Configure a TCP/IP Dial-Up Adapter Connection.
      • Interact Misc - Can ASCII register in the PLC be used as an alarm?
      • Configure a TCP/IP connection (IP address)
      • Compact Flash Disk Transfer using Interact MachineShop Toolbar to Upload and Download
      • ERROR - Invalid Panel list or Key Pad Address.
      • Ethernet download to a CTC Panel.
      • How to Restore Motion Panel.
      • Interact Software - Display alarms in a RMD tool within PTM
      • How to run app on my PowerStation on boot-up?
      • Implementing the New CMOT Driver
      • LEDs on the back of the Profibus card
      • MachineLogic - How do I clear Retentive Memory?
      • MachineLogic - No project on the PLC.
      • Security Key Setup not Installed
      • Single layer SST 5136-PFB-104 card with Interact.
      • TCP/IP Ethernet and a Dial-Up Connection
      • TCP/IP open port failure
      • Can I run Interact 6.X in Windows NT/2K/XP?
      • Can I run Interact7 on my Windows 10 or 7 PC?
      • Configure a TCP/IP connection (DHCP)
      • Configure a TCP/IP direct Ethernet connection
      • CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Enable/disable the screen saver
      • Flashback Utilities for the CTC DOS Based PowerStations - If you have Interact ver 7 it installs all the necessary Flashbacks.
      • HMI Battery Replacements
      • How do I connect my P13, PA or PA2 Interact HMI to DataHighway Plus Network?
      • How do I recalibrate my Interact touchscreen? Or change the panel's ethernet address?
      • How do I show hidden and protected files in Windows?
      • How do I transfer my old Interact application to a newer Interact panel?
      • How to connect my device to Interact? Interact Cable Dictionary
      • How to print graphics from Interact run mode.
      • I upgraded my old hardware to a PA2 and have Vertical Stripes on screen and does not load my application.
      • Interact does not recognize the security key.
      • Interact: Error Initializing AMM - Invalid Logging Path
      • Minimum of NT 4.0 SP3 to install Machine Shop
      • Powerstation Shell on older CTC units
      • Replacing old HMIs that run Interact
      • Upgrading from a PA to a PA2
      • What are Interact Runtime modules?
      • Whats the difference between FLH-0512P and FLH-0512?
      • What internal variable can I use to R/W ASCII?
      • Interact Troubleshooting - WinXP- cannot select options on Toolbar
      • Control Access to Panels and Tools using the Password User Levels in Interact
      • Driver for my Allen Bradley Micrologix 1500 PLC?
      • Fonts and Graphics on Tools broken after Interact Upgrade to Ver 7 to run on PA2 hardware. Application runs but FONT Size or images are wrong.
      • I need more fonts for my Interact application.
      • INTERACT How to Order
      • Interact screen size too BIG or too small after upgrade. Only see part of screen or screen compressed in top left corner of display.
      • Legacy Product Page - P1 Series
      • Legacy Product Page - P2 Series
      • Legacy Product Page - P3, P4, P5 and P7 Series
      • Security Key not found or Not programmed to support Module or Driver
      • Which HMI runs Interact?
    • InteractX+
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
Configure a TCP/IP Dial-Up Adapter Connection.

Print Friendly and PDF

Complete the following steps on the MachineShop Toolbar and MachineShop Shell:

MachineShop Toolbar

  • Right click on the 'Network Neighborhood' icon on the desktop and select 'Properties'. The 'Network' dialog will appear.

  • Select the 'Configuration' tab. The list will contain several items. Select the TCP/IP item for the Dial-Up Adapter (TCP/IP -> Dial-Up Adaptor) and click on the 'Properties' button. A message box containing a warning will appear.
    The text is as follows:

    "You have asked to change TCP/IP properties for a dial-up adapter. In most cases, these properties are unique to the specific network, which you are calling. For this reason, it is better to set TCP/IP properties in each connection icon, which calls a network. Otherwise, properties set for the adapter will override the per-connection settings. Connection icons can be found in the Dial-Up Networking folder under Start Accessories. Right click an icon to see its properties sheet; select Server Type, and then TCP/IP Setting."

    Click 'OK' on this message box. The 'TCP/IP Properties' dialog will appear.
  • The 'Obtain an IP address automatically' radio button should be selected (default configuration). If the 'Obtain an IP address automatically' radio button is not selected, select this radio button. The IP address, to be used, is configured in the Phonebook entry in Dial-up Networking.

  • Open the Dial-Up Networking folder by selecting 'Start Program Accessories Dial-Up Networking'. The 'MachineShop Phonebook Entry' dialog will appear.

  • Select the 'Server Types' tab. Click on the 'TCP/IP Settings' button. The 'TCP/IP Settings' dialog will appear.

  • The 'IP Address' radio button should be selected and the IP Address should be set to 10.0.0.1 (default configuration).


    MachineShop Shell:

    Using the PowerStation and the MachineShop Shell software, TCP/IP should be configured to exist on the same network as the MachineShop Toolbar. For example, if the IP Address of the MachineShop Toolbar is set to 10.0.0.1 and the Subnet Mask is set to 255.255.255.0; the PowerStation can be configured as follows (default configuration COM1):

  • IP Address: 10.0.0.2
  • IO Mask: 255.255.255.0
  • Interface: Serial
  • IRQ: 4
  • Port: 3F8h
  • Baud: 115200
  • INTERACT
  • Dial-Up Networking
  • Dial-Up
  • MachineShop Toolbar