Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Encoder Velocity
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Encoder Velocity
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
Encoder Velocity

Print Friendly and PDF

The Encoder Velocity Parameter is encoder pulses per servo interrupt. The default value of servo interrupt is 500 uSec so this is usually a very small number.

If you are trying to calculate velocity, see the sample program below:

REM ********************************************
REM Program to determine speed of source encoder
REM ********************************************
REM Be sure to allocate 1000 bytes of memory for Program


HALT
NEW
DETACH

AXIS1 ON
ATTACH MASTER1
ATTACH SLAVE0 AXIS1 "Y"

10 DIM LV2
20 P1=0
30 P4=0

100 INTCAP Y0 :REM Trigger INTCAP on marker
110 INH 809 :REM Assign P2 to value of Hardware capture register
120 P2=P12548 :REM Assign P5 to the value of Global system clock
130 P5=P6916

170 P3=(P2-P1):REM Determine pulses between marker pulse
180 P6=(P5-P4):REM Determine time (ms) between marker pulse

190 LV0=((1000/P6)*60):REM Calculate RPM


200 PRINT "Encoder count = ";P3;" * Time in mSeconds = ";P6
210 PRINT "RPM = ";LV0
220 PRINT " "

300 P1=P2
310 P4=P5
390 GOTO 100

REM ***** LRUN program to display information *****

Related FAQ:  How Fast is Servo Axis Moving?