Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Implementing the New CMOT Driver
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Implementing the New CMOT Driver
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
  • Visualization and Human Machine Interface (HMI)-
    • Interact (Legacy)-
      • Replace/Upgrade Interact panel P11/P1H/P15/P2/P3/P4/P5 etc
      • CTC and i-Motors
      • Configure a TCP/IP Dial-Up Adapter Connection.
      • Interact Misc - Can ASCII register in the PLC be used as an alarm?
      • Configure a TCP/IP connection (IP address)
      • Compact Flash Disk Transfer using Interact MachineShop Toolbar to Upload and Download
      • ERROR - Invalid Panel list or Key Pad Address.
      • Ethernet download to a CTC Panel.
      • How to Restore Motion Panel.
      • Interact Software - Display alarms in a RMD tool within PTM
      • How to run app on my PowerStation on boot-up?
      • Implementing the New CMOT Driver
      • LEDs on the back of the Profibus card
      • MachineLogic - How do I clear Retentive Memory?
      • MachineLogic - No project on the PLC.
      • Security Key Setup not Installed
      • Single layer SST 5136-PFB-104 card with Interact.
      • TCP/IP Ethernet and a Dial-Up Connection
      • TCP/IP open port failure
      • Can I run Interact 6.X in Windows NT/2K/XP?
      • Can I run Interact7 on my Windows 10 or 7 PC?
      • Configure a TCP/IP connection (DHCP)
      • Configure a TCP/IP direct Ethernet connection
      • CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • Enable/disable the screen saver
      • Flashback Utilities for the CTC DOS Based PowerStations - If you have Interact ver 7 it installs all the necessary Flashbacks.
      • HMI Battery Replacements
      • How do I connect my P13, PA or PA2 Interact HMI to DataHighway Plus Network?
      • How do I recalibrate my Interact touchscreen? Or change the panel's ethernet address?
      • How do I show hidden and protected files in Windows?
      • How do I transfer my old Interact application to a newer Interact panel?
      • How to connect my device to Interact? Interact Cable Dictionary
      • How to print graphics from Interact run mode.
      • I upgraded my old hardware to a PA2 and have Vertical Stripes on screen and does not load my application.
      • Interact does not recognize the security key.
      • Interact: Error Initializing AMM - Invalid Logging Path
      • Minimum of NT 4.0 SP3 to install Machine Shop
      • Powerstation Shell on older CTC units
      • Replacing old HMIs that run Interact
      • Upgrading from a PA to a PA2
      • What are Interact Runtime modules?
      • Whats the difference between FLH-0512P and FLH-0512?
      • What internal variable can I use to R/W ASCII?
      • Interact Troubleshooting - WinXP- cannot select options on Toolbar
      • Control Access to Panels and Tools using the Password User Levels in Interact
      • Driver for my Allen Bradley Micrologix 1500 PLC?
      • Fonts and Graphics on Tools broken after Interact Upgrade to Ver 7 to run on PA2 hardware. Application runs but FONT Size or images are wrong.
      • GESNP / GESNPX 9030 / 9070 Serial Com configuration for Interact / PowerStation PA/PA2/P13 etc...
      • I need more fonts for my Interact application.
      • INTERACT How to Order
      • Interact screen size too BIG or too small after upgrade. Only see part of screen or screen compressed in top left corner of display.
      • Legacy Product Page - P1 Series
      • Legacy Product Page - P2 Series
      • Legacy Product Page - P3, P4, P5 and P7 Series
      • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
      • Security Key not found or Not programmed to support Module or Driver
      • Which HMI runs Interact?
    • InteractX+
    • Interact Xpress+
    • IXA / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (Discontinued)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • What CF Card do I need? And my HMI will not boot. Says no boot device found even after running the Flashback utility for my HMI model
    • Latest versions of HMI software packages
    • PFD - Parker Factory Display (Discontinued)+
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Implementing the New CMOT Driver

Print Friendly and PDF

If you find that you need to upgrade your version of the CMOT driver for the CTC panel then follow the procedure below. For this procedure you will need a Flash Disk Reader and a keyboard on top of the CTC panel. Also, this procedure will remove the existing application from the flash card. You should upload it to the computer before proceeding.

First, download the newest flashback utility from www.CTCUSA.com. Click on support, then Utilities, then download the "P1-P7 & PS Series MachineShop Shell Flashback Utility (New Shell) for all units." DO NOT DOWNLOAD THE FLASHBACK UTILITY THAT INSTALLS THE MOTION PANEL APPLICATION BECAUSE THIS WILL NOT INSTALL THE NEW SHELL!

Power down the CTC panel and remove the flash card from the side. Put the flash card into the flash card reader attached to your computer. The double-click on the flash utility you just downloaded and run the executable file inside the zipped file. Select the drive letter for which the flash card reader resides and then hit restore flash.

Once this is complete got back to www.CTCUSA.com and click again on support, then software information, then drivers and finally B-C. Then scroll down to find Compumotor and the CMOT driver. Download this file and extract it to the following directory:

C:\MachShop\Ineract\Drivers\CMOT

Make sure to choose to over-write the existing files. To ensure that you have replaced the CMOT driver with the newer version, go to the above directory on your hard drive and right-click on CMOT.dll. Select properties, and then go to the version tab and the highlighted number should something like this "EX-82998-604;" this signifies version 6.04 of the CMOT driver. This number should be the same as the one from CMOT.dll in the zip file you downloaded.

After this is done, download your project to the flash card from Machine Shop.
After downloading your project, place the flash card back into the CTC panel, plug your keyboard to the CTC panel and power it up. Since all of the parameters are set back to defaults, you will have to reconfigure the CTC panel. When you power the unit up, it will go to the Machine Shop Shell; this is where all communications are setup for the CTC panel.

First go to Settings, and then General; select Power On Operation and finally Run Interact. This will ensure that Interact will automatically run on power up.

Select back, then settings again. This time select TCP/IP and make sure that TCP/IP is enabled. If it is not, then enable it. Then select Net Setup. If you are using COM1 then all you need to change is the Baud Rate to 9600. But if you are using Ethernet then the following settings must be made:

IP Address 192.168.10.29 (default, must be on Net 1)
IP Mask 255.255.255.0
Interface Type NE2000 (Use I82557 for PS series)
IRQ 10
PORT 280h

After you have made these settings, select back twice and it will ask you if you want to the reboot the unit. Select yes and you are done.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply