Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base 6K Accessories - Using a thumbwheel with my 6000/6K controller?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base 6K Accessories - Using a thumbwheel with my 6000/6K controller?
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
  • Motion and Machine Controllers-
    • ACR Controllers+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)-
      • 6K Accessories - Connector Part Numbers
      • 6K Accessories - Connector Part Numbers for Older Model PS-60W
      • 6K Accessories - Do I have a SIM8-OUT-SSR or SIM8-OUT-HCR?
      • 6K Accessories - Drive Command Cable
      • 6K Accessories - DVT and 6K Details
      • 6K Accessories - EVM32 "GND" and "RTN" connections
      • 6K Accessories - EVM32 and SIM card compatibilities
      • 6K Accessories - EVM32 max cable length
      • 6K Accessories - External Third Party I/O Modules
      • 6K Accessories - Joystick Options.
      • 6K Accessories - Operating Voltage for EVM32-II Output Relays
      • 6K Accessories - OPTO22 to 6K Analog Units
      • 6K Accessories - USB-to-serial Adapters with Motion Planner
      • 6K Accessories - Using a thumbwheel with my 6000/6K controller?
      • 6K Hardware - Analog Input Resolution
      • 6K Hardware - Flash Memory Limitation and Battery Backed RAM
      • 6K Hardware - How to Connect an Older Parker Step Motor's Encoder (-E Option) to 6K
      • 6K Hardware - Maximum encoder input frequency
      • 6K Hardware - Where is the OUTDIODE connection?
      • 6K Misc - Automating the ARP -S Procedure
      • 6K Misc - Battery Replacement for 6K & 6000 Series Products
      • 6K Misc - Can the 6K accept multiple Ethernet connections?
      • 6K Misc - Command Cross Reference (6K to ACR)
      • 6K Misc - Communication Protocols
      • 6K Misc - Completely Reset the 6K to Factory Default via Hardware
      • 6K Misc - Completely Reset the 6K to Factory Default via Software
      • 6K Misc - Connecting a Motion Panel to a 6K.
      • 6K Misc - Connecting to the Gemini and the 6k simultaneously
      • 6K Misc - Creating 6K Backup Programs
      • 6K Misc - Custom 6K Firmware (no longer quoting new 6K custom features)
      • 6K Misc - Daisy Chaining with 6000 or 6K products
      • 6K Misc - Ethernet (TCP/IP) Communications via HyperTerminal.
      • 6K Misc - Ethernet Client Capability
      • 6K Misc - Ethernet equipment needed for communication?
      • 6K Misc - Feedrate Override in the 6K.
      • 6K Misc - Fieldbus Data Transfer Rates
      • 6K Misc - How can I download my 6K ops without Windows?
      • 6K Misc - Is the 6K UL Recognized?
      • 6K Misc - Letter of Volatility
      • 6K Misc - Limits/Home Inputs on 6K2
      • 6K Misc - Motion Planner Minimum Requirements (not compatible with Win10 or later)
      • 6K Misc - MX80L with ViXnnnAH and 6K Notes
      • 6K Misc - Necessary files for Motion Planner.
      • 6K Misc - OS Firmware and Hardware Compatibility (6K, GT6K, GV6K)
      • 6K Misc - Outputs on Position (OUTP Command)
      • 6K Misc - Serial Communication Protocols.
      • 6K Misc - Serial Communications
      • 6K Misc - Servo Update Rate
      • 6K Misc - Target Zone bit with Stepper
      • 6K Misc - Tuning 6K and Gemini--Starting Parameters
      • 6K Misc - What is Saved in the 6K memory (Non-Volatile Memory)?
      • 6K Misc - Windows NT/2000/XP and NTFEN
      • 6K Software - Assigning a variable value to an analog output
      • 6K Software - Assigning Binary Variables (Varb)
      • 6K Software - Binary Variables (Varb)
      • 6K Software - Changing Outputs with Compiled Motion.
      • 6K Software - Com6srvr for Large File Sizes
      • 6K Software - Command processing in the 6K with SYSPER.
      • 6K Software - Compatibility with Motion Toolbox or Motion OCX
      • 6K Software - Connecting to 6K with Visual Basic
      • 6K Software - Connecting to the 6K with Visual C++
      • 6K Software - Does a !K Command Stop a PLC program?
      • 6K Software - Example program for general motion
      • 6K Software - Following a Virtual Master
      • 6K Software - HALTing a Task.
      • 6K Software - Home to Z Channel for Rotary Applications
      • 6K Software - How do I use Scaling in the 6K
      • 6K Software - How long does the 6K take to execute commands?
      • 6K Software - How to disable the power-up banner message
      • 6K Software - How to use the Com6Srvr with LabView
      • 6K Software - INFNC Program Selection
      • 6K Software - LabVIEW / Motion Toolbox Products
      • 6K Software - Minimum distance per compiled segment
      • 6K Software - Motion Planner and Visual Basic Script (not Win10 compatible)
      • 6K Software - PLCP Execution.
      • 6K Software - Position Maintenance Mode
      • 6K Software - PPRO Scaling
      • 6K Software - Reading Analog Inputs with the Com6srvr
      • 6K Software - Rounding Variables in 6000 or 6K Products
      • 6K Software - Running Motion Planner on Windows 7 or Windows 10?
      • 6K Software - Sending Commands via RS232
      • 6K Software - TASF Bit 1 -- Moving/Not Moving
      • 6K Software - TASF Bit 28 -- Registration Move
      • 6K Software - TASF Bits 24 & 25 -- Target Zone
      • 6K Software - Task Swapping (Multi-tasking Feature)
      • 6K Software - Updating the com6srvr.exe file
      • 6K Software - Using the Com6srvr as an ActiveX (OCX) component.
      • 6K Software - Using the Com6srvr without Motion Planner.
      • 6K Software - Using the LIMFNC command for Limits and Home.
      • 6K Software - Where is the Communication (com6srvr) server located?
      • 6K Software - Why do I get a *B and *C when I turn on my 6K?
      • 6K Training - Express Basics Training: How to Connect Ethernet - includes Win7 (VIDEO)
      • 6K Training - Express Basics Training: How to upload & download to 6K controllers (VIDEO)
      • 6K Troubleshooting - Cannot Connect to DVT Camera After Reset or Power Cycle
      • 6K Troubleshooting - Com6Srvr uses 100% of CPU
      • 6K Troubleshooting - EFAIL Command Clarification
      • 6K Troubleshooting - Encoder Input Impedance
      • 6K Troubleshooting - How do I know what error started the ERROR Program
      • 6K Troubleshooting - I cannot ARP -S in Win95
      • 6K Troubleshooting - I cannot read the encoder position (Com6srvr)
      • 6K Troubleshooting - KDRIVE1 does not disable drive on a stall
      • 6K Troubleshooting - Master Slave Distance Mismatch Error (Following)
      • 6K Troubleshooting - Memory Errors in Stand-Alone Products.
      • 6K Troubleshooting - Motion Panel Loses Communication Periodically
      • 6K Troubleshooting - Motion Planner/Communication Server
      • 6K Troubleshooting - My .TLB file does not work (Com6srvr)
      • 6K Troubleshooting - My 6K locks up during a download.
      • 6K Troubleshooting - My 6K stops when I cut power to my EVM32.
      • 6K Troubleshooting - My ethernet is locking up.
      • 6K Troubleshooting - My servo motor is not moving.
      • 6K Troubleshooting - No Remote Panel Error or Power-Up Sequence Failure
      • 6K Troubleshooting - RS232 Troubleshooting for 6K / 6000 Products
      • 6K Troubleshooting - Scrolling Carrots with Motion Panel and 6K
      • 6K Troubleshooting - SSLex0105e: Invalid token, Line 1, Offset 10, <<
      • 6K Troubleshooting - Stalling due to Mechanical Backlash
      • 6K Troubleshooting - TASF Bit 12 -- Stall Detected
      • 6K Troubleshooting - TASF Bit 13 -- Drive Shutdown
      • 6K Troubleshooting - TASF Bit 14 -- Drive Fault Occurred
      • 6K Troubleshooting - TASF Bit 15 & 16 -- Hardware Limit Hit (End of Travel Limits)
      • 6K Troubleshooting - TASF Bit 23 -- Position Error Exceeded
      • 6K Troubleshooting - TASF Bit 26 -- Motion Suspended
      • 6K Troubleshooting - TASF Bit 30 -- Move Not Possible
      • 6K Troubleshooting - TASF Bits 17 & 18 -- Software Limits Hit
      • 6K Troubleshooting - TASX Bit 4 -- Drive Fault Input Active
      • 6K Troubleshooting - TASX Bit 5 -- Encoder Failure
      • 6K Troubleshooting - The ARP entry addition failed: 5
      • 6K Troubleshooting - The Panels do not work (Motion Planner)
      • 6K Troubleshooting - Turning off my computer stops my program.
      • 6K Troubleshooting - VBScript panels will not run (Win7 or before only - not compatible under Win10)
      • 6K Troubleshooting - Visual Basic run-time error 2147418107
      • 6K Troubleshooting - Why am I having 6K program download or upload problems?
      • 6K Troubleshooting - Why does the 6K not see my drive fault?
      • 6K Troubleshooting - Why does the Com6srvr use 100% of the CPU?
      • 6K Troubleshooting - Why is my analog input card not working properly?
      • 6K Troubleshooting - Why STARTP will not always work.
      • 6K Troubleshooting - Write Command in a Program While Using Port 2 (doesn't display on the terminal or other device)
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
6K Accessories - Using a thumbwheel with my 6000/6K controller?

Print Friendly and PDF

Compumotor originally had its own thumbwheel, known as the TM8, which had 8 numeric thumbwheels and one sign thumbwheel. The TM8 contained a 3-to-8 line decoder which allowed 3 outputs from a controller to select one of the 8 thumbwheels to strobe. In addition, the TM8 only required 4 inputs (5 inputs if the sign thumbwheel was used)on the controller, since only one thumbwheel was strobed at one time.  Note - TM8 product line is no longer offered.

The TM8 had its own unique command set which took advantage of the 3-to-8 line decoder. These thumbwheels commands are only for the TM8 thumbwheel, and will not work with other thumbwheels. The INSTW command configures the inputs of the controller to be thumbwheel inputs used with the TM8 exclusively. The OUTTW command configures the outputs of the controller to be thumbwheel outputs used with the TM8 exclusively. The TW command is used to read the thumbwheel inputs. TW sets 1-4 are used with the TM8 only (sets 5-8 are for the PLC commands).

When using any other thumbwheel,or when requiring parallel data transfers from PLC I/O to the controller, you use a second set of commands. The INPLC command configures the inputs to receive BCD formatted data. The OUTPLC command configures the outputs to be strobed for a specific amount of time, which determines where data on the inputs will be stored. The TW command is used to read the PLC (thumbwheel) inputs. TW sets 5-8 are used with the PLC inputs (sets 1-4 are used for the TM8 commands). The thumbwheel inputs can be stored in 4 sets of numbers. Thus, the same thumbwheel can be used to represent four different values. When using INPLC1 and OUTPLC1, use the TW5 command to read the data. When using INPLC2 and OUTPLC2, use the TW6 command to read the data.When using INPLC3 and OUTPLC3, use the TW7 command to read the data. When using INPLC4 and OUTPLC4, use the TW8 command to read the data.

The INPLC and OUTPLC commands were designed to be used with a specific number of inputs and outputs in mind. Since the data is read in as BCD inputs and a thumbwheel traditionally has digits 0 through 9, the number of BCD inputs required per thumbwheel is 4. However, each time one output is strobed, two digits of information are stored on the controller. Therefore, the anticipated configuration of I/O when using a thumbwheel required 8 inputs and 4 outputs (two thumbwheels read per output strobed).



The following is an example of how it works:

INPLC1,1-8,0,0
OUTPLC1,1-4,0,500
THUMBWHEEL: 12345678
VAR1=TW5

We have an 8 digit thumbwheel, with inputs 1-8 defined as the data inputs and outputs 1-4 defined as the strobing outputs. We are going to store the values of the thumbwheel into set 1, thus we will use the TW5 command, and assign it to VAR1 by using the command VAR1=TW5. The resulting value when we query VAR1 is 0.12345678 (notice that all the digits are to the right of the decimal point). When we assign a distance by commanding a D(TW5), and query D, the result is D+12345678 (notice that there is no decimal in this number when scaling is off SCALE0). When we assign a velocity by commanding a V(TW5), and query the V, the result is V+1234.5678 (notice that there is a decimal in the number, with 4 decimal places when scaling is off SCALE0).
Since D, V, and A are scalable, the location of the decimal in the value depends upon their respective scaling factors (SCLD, SCLV, & SCLA).

When output1 is strobed (OUT1 turns on) for 500ms, it will place the BCD equivalent value of Inputs 1-4 (Input 1 is the LSB and Input 4 is the MSB) into the second digit from the left most position, in our example it is 2. Simultaneously, it places the BCD equivalent value of Inputs 5-8 (Input 5 is the LSB and Input 4 is the MSB) into the left most position, in our example it is a 1. VAR1=0.12000000. Now, output1 is turned off, and output2 is strobed (OUT2). The BCD eqivalent value of Inputs 1-4, 4, is placed in the 4th position from the left and, simultaneously, the value of Inputs 5-8, 3, is placed in the 3rd position from the left. VAR1=0.12340000. Next, output2 is turned off, and output3 is strobed (OUT3). The BCD eqivalent value of Inputs 1-4, 6, is placed in the 6th position from the left and, simultaneously, the value of Inputs 5-8, 5, is placed in the 5th position from the left. VAR1=0.12345600. Lastly, output3 is turned off, and output4 is strobed (OUT4). The BCD eqivalent value of Inputs 1-4, 8, is placed in the 8th position from the left and, simultaneously, the value of Inputs 5-8, 7, is placed in the 7th position from the left. VAR1=0.12345678.

As in the figure above, as you decrease the number of outputs, the data shifts to the right. Thus, if only 1 output is used, it will place the data into the 7th and 8th positions, preceded by 0's as place holders. If less inputs are used, i.e. only Inputs 1-4, then 0's will be placed in the Input 5-8 locations. VAR1=0.02040608.