Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Why will my PAD and PED not update on the Gemini?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Why will my PAD and PED not update on the Gemini?
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)-
      • 24 Volt Keep Alive
      • Analog input on GV6, GV6K, GT6, GT6K
      • Audible Noise in Stepper Motors
      • Cable breakout modules for the Gemini
      • Can I run the MX80L using a Gemini Drive?
      • Can the Gemini Products take a DC voltage supply?
      • Changing Motor direction on the GV6 or GT6
      • Chopping frequency of the Gemini drive.
      • Connector Part Numbers
      • Controller to GV Cables
      • Currently Released Gemini Drive Products
      • Daisy chaining GVs and GTs
      • Digital Notch Filters
      • Does the Gemini drive have a test mode?
      • Downloading the OS to my Gem6K locks up.
      • Encoder Motors Work with Gemini Resolver units
      • ERES /ORES Relationship for Gemini GV Products
      • GC-SDA Fault output is not really the fault output
      • GEM-VM50 screw-terminal breakout dimensions
      • Gem6K (GV6K & GT6K) Family Letter of Volatility
      • Gemini MaxPlus (MPM) Resolver Option 1 Connection
      • Gemini - Downloading in
      • Gemini - MaxPlus (MPM) Encoder Option 1 Connection
      • Gemini - MaxPlus (MPM) Encoder Option 5 Connection
      • Gemini Analog Input Deadband
      • Gemini Analog Output A now dithers
      • Gemini GV - Resolver to Encoder Signal Conversion
      • Gemini GV6 & GT6 RS232 Daisy-Chaining ERRLVL
      • Gemini Maximum Frequency Input and Output
      • Gemini OS Download Failures
      • Gemini Step & Direction Inputs
      • Gemini Update Rates.
      • Gemini Variable Resolution
      • Gemini: 400LXR Tuning
      • Gemini: ASCII or Binary?
      • Gemini: VIDEO: express basics training: How to Connect Ethernet (includes Win7)
      • Getting the letter a with a ~ over it in Motion Planner Terminal
      • GFB-KIT Pinout
      • GV Cable Diameters.
      • GV6K & GT6K cannot Follow Analog Onboard Input
      • GV6K Tuning in Position Mode with Motion Planner
      • Hall State Checking on Gemini Products
      • Hall-less Startup on Gemini
      • I cannot communicate with my GEM-6K.
      • Limits on Gemini
      • MS cable option vs. GS cable option
      • OS 1.70 Additions
      • Replacing the Gemini GC-SDA
      • RESET command in STARTP program
      • Resolution of the Gemini command signal.
      • RS232 Troubleshooting for the Geminis
      • Step & Direction Output
      • TASX Bit 1 -- Motor Temperature Fault
      • TASX Bit 10 - Bridge Fault (Hardware)
      • TASX Bit 11 -- Bridge Over-Temp Fault (Software)
      • TASX Bit 12 -- Over-Voltage Fault
      • TASX Bit 17 -- Stall Detected
      • TASX Bit 18 -- Override mode
      • TASX Bit 19 -- Foldback Active
      • TASX Bit 2 -- Low Voltage Fault
      • TASX Bit 20 -- Power Dissipation Circuit Active
      • TASX Bit 21 -- Bad Hall State Detected
      • TASX Bit 22 -- Unrecognized Hardware Detected
      • TASX Bit 23 -- User Fault Input Active
      • TASX Bit 24 -- Keep Alive Circuit Active
      • TASX Bit 25 -- Power Dissipation Circuit Fault
      • TASX Bit 28 -- Motor Configuration Warning
      • TASX Bit 29 -- ORES Failure
      • TASX Bit 3 -- Drive Temperature Fault
      • TASX Bit 30 -- Motor Thermal Model
      • TASX Bit 31 -- Commanded Torque Limit Hit
      • TASX Bit 5 -- Encoder/Resolver Failed
      • TASX Bit 7 -- Motor Configuration Error
      • TASX Bit 8 -- Incoming Pulses
      • TASX Bit 9 -- Velocity Error Limit Exceeded
      • The GV and Linear Motors
      • Tuning a GV6K GV6 or GV in Position Mode
      • Tuning GV or GV6 drives with large inertia loads.
      • Tuning the Gemini in Position Mode
      • Tuning the Gemini in Position Mode.
      • Tuning the Gemini in Torque Mode.
      • Tuning the Gemini in Velocity Mode.
      • Using Gemini with Empire Magnetics Step Motors
      • VIDEO: Basics Training: GV or GT drives
      • VIDEO: Basics training: GV6 or GT6 drive controllers
      • VIDEO: Basics training: GV6K or GT6K drive controllers
      • What are Q and D currents?
      • What does the Error Log contain?
      • What drives can work with a DC brushed motor?
      • What happens in Keep Alive mode?
      • What motors with what Gemini drive?
      • What recognitions does the Gemini GV have?
      • What replaces the Gemini GT stepper drive?
      • What replaces the Gemini GT6 stepper drive/controller?
      • What replaces the Gemini GT6K stepper drive/controller?
      • What replaces the Gemini GV6K servo drive controller?
      • Which Motors Work with GV-L Drives? GV-U Drives?
      • Which rotation is considered positive for GV6K?
      • Why doesn't my Drive I/O cable tighten down securely when using the jackscrews?
      • Why will my PAD and PED not update on the Gemini?
      • Z channel output from the Gemini?
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Why will my PAD and PED not update on the Gemini?

Print Friendly and PDF
The commands, FBPIC and FBPOC setup the cyclic part of the Profibus data packet. Basically, they state what information the PAD and the PED of the data packet will represent.

These commands will NOT properly execute when placed inside a program. One must either type the commands in at the terminal, or place them before the first DEL in the program file (.prg). It is acceptable to place them inside a program, so on upload the values for FBPOC and FBPIC will be seen. But, upon download, they need to be copied outside of the program so they are properly executed.

Also, for the new settings to take place, a RESET command (or power cycle) must be issued.

What complicates things more, is if one inserts the two commands in a program, but does not type the two commands in at the terminal or does not type them outside of the programs in the Program file (.prg), the values of FBPIC and FBPOC will falsely report back the new values. So, when they query the FBPIC and FBPOC commands, they report back the values as set in the program file they downloaded. However, the actual proper execution of the commands did not happen, so they are not properly configured on the drive.

As an example, if FBPOC and FBPIC are set to 0,0,0,0 and you download a program with the commands FBPIC1,2,0,0 and FBPOC1,2,0,0 to the controller, FBPIC and FBPOC will not change until you execute PROG1 and do a RESET (power cycle). Once PROG1 and the Reset are executed, FBPOC and FBPIC will change in value. Thus, when queried, FBPOC and FBPIC will report back 1,2,0,0. However, when checking those bits over the Profibus, they will not update and have no function. If you now type FBPIC1,2,0,0 and FBPOC1,2,0,0 in the terminal and do a RESET (power cycle), the bits of the Profibus will now work properly.
Sample Program (.prg):

FBPIC0,2,0,1 ;sets the PAD to report Actual Speed & Position
FBPOC3,0,0,1 ;sets the PED to accept Acceleration & Postion
DEL PROG1 ; deletes a program called PROG1
DEF PROG1 ; defines a program called PROG1
LH0 ; disable both limits
MC0 ; set to preset mode (mode continuous off)
MA0 ; set to incremental mode (mode absolute off)
END; end of the program PROG1

DEL PROG2 ; deletes a program called PROG2
DEF PROG2 ; defines a program called PROG2
L0 ; setup an infinite loop
D25000 ; set distance to 25000 units
V(VARI1) ; set the velocity to equal the value of VARI1
GO1 ; make motion
WAIT(AS.1=b0) ; wait for motion to complete
WAIT(IN.5=b1) ; wait for input 5 to go active
LN; end of the infinite loop
END; end of the program PROG2
STARTP PROG1; assign PROG1 to the Startup Program
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply