Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Operating System Update Notes
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Operating System Update Notes
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)-
      • Controller (CE)+
      • Drive only (AE,AR, SE, SR)-
        • 3rd party resolver with resolver based Aries drive
        • Aries ARxxSE/ARxxSR tuning for Step/Direction
        • Aries Drive Family Letter of Volatility
        • Aries encoder output - Quadrature or SSI?
        • Galil DMC to Aries Connections
        • Hall-only Commutation
        • Meaning of the Status LEDs
        • Operating System Update Notes
        • RS485: PC connections through B&B Electronics 485BAT3 to Aries
        • Using single-ended inputs with the Aries
        • VIDEO: How to Configure Aries Servo Drives
        • What does it mean when my left LED is flashing 1 yellow and 5 green?
        • Why are Aries motor parameters missing?
        • Why is my Aries torque-drive clicking?
        • Why is my enable LED flashing?
        • Why is there a delay before motion on my Aries?
      • EPL+
      • AR-20 and AR-30 minimum AC voltage
      • Absolute Encoders & Drive Compatibility
      • Aries - MaxPlus (MPM) Encoder Option 1 Connection
      • Aries - MaxPlus (MPM) Resolver Option 1 Connection
      • Aries Brake Delay
      • Aries Drive: Connector Part Numbers
      • Bayside GM Gearmotor Files for Aries
      • Cables to connect GM motors to Parker Drives
      • Can I use Aries drives with MX80L linear motor stages?
      • DTALK with Aries 3.32 & higher firmware
      • E27 Bridge Hardware Fault
      • E54 Feedback Loss Fault - 5 Green Flash 1 Yellow
      • How do I power an ARIES with 3 phase?
      • How do I know Aries SFB is set to auto-detect?
      • How to Update Operating System (Firmware)
      • Manual Alignment Procedure
      • Peak Current Time from Compumotor Drives
      • Aries drive won't enable
      • Selecting a Fuse
      • Using R100,R150 and R200 with Aries
      • Aries (AR-xxAE or AR-xxSE) Recommended Replacements
      • Aries 2000/3000 watt Replacements (AR-20AE, AR-30AE, AR-20SE, AR-30SE)
      • Aries Resolver Replacement (AR-01AR, AR-02AR, AR-04AR, AR-08AR, AR-13AR, AR-01SR, AR-02SR, AR-04SR, AR-08SR, AR-13SR)
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Operating System Update Notes

Print Friendly and PDF


Please note that Aries Support Tool 3.1.0 has a Terminal Emulator screen. 

When connected to the Aries with power on, with a red flashing LED, you will see the letter C to start to appear in the Terminal Emulator screen. 

This means you are connected correctly to the Aries. 
If you are not seeing the letter C, double-check the RS232 wiring. 
On a standard 9pin PC Com port, pin2 is the computer's receive and should be connected to Tx (pin26).
On the 9pin PC Com port pin3 is the computer's transmit and should be connected to Rx (pin25).
Pin5 on the PC is Ground and should be connected to Gnd (pin24).

To confirm you are connected to the COM port, perform a loop back test to confirm you're connected to the COM port. 

Perform a "Loop Back" test to verify that your serial cable is working:
1. Disconnect Rx and Tx from the Aries
2. Short Rx and Tx wires together
3. On the Aries Support Tool, click on the Terminal Emulator screen
4. While these two connections are shorted, type any characters
5a. If you do not see any of these characters: Either you have a bad cable, you chose the wrong COM port, or your COM port is damaged.
5b. If you do see characters, but not able to connect to the Aries, then Rx and Tx are swapped. Reverse the Rx and Tx wiring connections.
When the Aries has a red flashing LED, the Com Connections test on the main screen in the Aries Support Tool will not work. (Note that the only way to get to a red flashing LED, the drive would've had to been connected at some point.)

Under Operating System Update, click Download Operating System. Locate the .ops file. It's a good idea when running this, that this file reside on your PC and not on a network server. 

A status bar is shown as the operating system is being updated with both the yellow and red led's flashing. The AST reports when this is complete that the operating system was successful.

Don't interrupt this download. However, if this is interrupted on accident, such as an intermittent serial connection, the status bar won't be increasing and the leds are still red and yellow. Cycle power on the Aries. You will then have a red flashing led. Then start the operating system download again.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply