Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base System Pointer Address of ACR Global Variables, P0-P4095
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base System Pointer Address of ACR Global Variables, P0-P4095
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
System Pointer Address of ACR Global Variables, P0-P4095

Print Friendly and PDF

Supplement to ACR Programmers Guide,Binary Host Interface "Application: Binary Global Parameter Access"

The memory address for the global user variables (P0-4095) can be read at the "System Pointer Address" Each controller has a different address based upon it's firmware:

AR-xxCE  0xA0600020
ACR9000 0x400009     (same for 9030,9040,9600,9630,9640)
ACR8020 0x400009
ACR8010 0x403E08
ACR8000 0x403E08
ACR2000 0x400008
ACR1505 0x400009
ACR1500 0xC08008
ACR1200 0x400008

This could be used with the ComACRserver's "GetACRMemory" to retrieve the value of up to 255 global variables at a time.

Using the GetACRMemory for the above address retrieves the Global_Variable_Address. 

If the returned address is zero, there are no dimensioned global variables (see the DIM command).

If the returned address is other than zero, use GetACRMemory at this address to receive the number of dimensioned global variables.

Read a global variable P(index) using the following addressing scheme for Peek: 

Peek address = Global_Variable_Address + 1 + ( index * 2 )
Where index = 0 to ( number of dimensioned global variables - 1 )

Even though global variables are stored on-board as floating point 64 (FP64) numbers, they are returned as IEEE32 numbers.
 
Note for Aries Controller (AR-xxCE), all memory accesses are byte addresses, so the equation to access globals on the CE is different:
Peek address = Global_variable_address + 4 + (index*8), where index = 0 to (number of globals-1).
 
Update 23-Mar-2012 JW
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply