For customers that wish to use an S/SX or ZETA product with the L20, Compumotor recommends the following solutions:
S/SX Series:
Pre anti-resonance drives will operate fine (see serial numbers below). S/SX drives with anti-resonance already installed should not be modified in the field. For more information contact Compumotor Applications Engineering Department.
Future orders of S/SX drives for linear motor applications should use the following new part numbers:
CP-S6-DRIVE-L20
CP-SX6-DRIVE-L20
CP-SXF6-DRIVE-L20
ZETA:
Both anti-resonance and active damping should be disabled.
(Electronic viscosity will still function properly.)
Models with serial numbers greater than or equal to those listed below, have anti-resonance installed.
S6 S/N 95062300253
S8 S/N 95062300062
SX(F)6 S/N 95071200321
SX(F)8 S/N 95071800091