Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Sample Program - Move Continuously, Stop on Inputs
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Sample Program - Move Continuously, Stop on Inputs
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)-
      • Analog control of a Vix stepper
      • Can an Intelligent ViX-In be Programmed as a Drive
      • Configuring the ViX-drive
      • DC Brushed Motor with a ViX
      • Does the Vix have software limits?
      • Downloading Programs
      • Easi-V with Windows 7 or Windows 10
      • Homing move not complete
      • How Do I Check encoder position?
      • How to program an intelligent ViX Stepper as a Step & Direction
      • LOADENC and SCALE Commands
      • Running a Rotary Motor with a ViX-xH
      • Sample Program - Move Continuously, Stop on Inputs
      • VIX - RS232 connections
      • VIX Servo: How to Home to a Hard Stop
      • VIX Update Rates
      • ViX User Variables
      • ViX CANopen / RS-485 option
      • ViX Easi-V Error Message: Invalid data read for limits mode
      • ViX Encoder Resolution / Input Frequency
      • ViX Motor files for non-preferred BE windings
      • ViX Tuning
      • ViX servo drive Z channel encoder output
      • ViX-RJ45 RS-232 Daisy-Chain Cables
      • ViX: Connector Part Numbers
      • ViX: ViX Update Rates
      • Vix- Option 1 (MPM) Encoder Hardware Setup
      • Vix-IE with Brushed motor and Encoder
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Sample Program - Move Continuously, Stop on Inputs

Print Friendly and PDF

MC is used for continuous motion. Below is a sample program.

The D4000 command sets the direction based on the sign of the numeric value; a D-4000 would set the direction as negative. The numeric value itself is irrelevant in MC, only the sign is important.

To stop on an input condition, first initiate motion and then LOOP another subprogram that does nothing but check for the inputs.

In order to be able to use the TR command after motion has been commanded change the setting of the CQ system variable. Setting the CQ to 0 will allow the processor to command motion and then execute subsequent commands like TR. This is similar to setting COMEXC1 in the 6K/6000 language.

1L1:

1W(CQ,0)

1A10

1V10

1MC

1D4000

1G

1LOOP(CHECK,0)

1END

1CHECK:

1TR(IN,=,1XXXX)

1S

1END

1SV

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply