Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base How to Find Torque or Current commanded from ACR
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base How to Find Torque or Current commanded from ACR
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
How to Find Torque or Current commanded from ACR

Print Friendly and PDF

Actual Torque is reported from the drive into the ACR90x0's "Final Output Signal" parameter (p12319 for Axis0). In Numeric status, it is under Axis Parameters > Monitor Parameters > Final Output Signal. . This is the equivalent of a DAC output value so that +10 is the max (equal to 100% of DMTLIM/DMTSCL for AriesEPL) and -10 is the minimum (-100% of those settings). Multiply by the drive's current scaling to calculate the current demand. To convert from current to motor torque, multiply by the motor's torque constant (typically the Kt value which is amount of torque per Amp). Or for the Aries or Gemini drives, just multiply the Final Output by the DMTSCL.


Compax3-EPL:
When monitoring the 'Final Output Signal' in the ACR9xx0 for a Compax3 axis on EPL, this maps to C3 object 683.1 (EPL object 0x6077) and is "% rated current."

Divide the Final Output Signal by 0.30517 to give fraction of rated current (A factor of 0.30517 is being applied in the firmware.) Divide by 100 as % rated current.

For current: Multiply resultant by C3 ServoManager's Rated Current (at 230, 400 or 480vac). This is the motor's rated current at rated speed, not the stall current (at 0 speed) which drops at higher speed due to spinning losses.

For torque: Multiply resultant by C3 ServoManager's Rated Torque (at 230, 400 or 480vac). This is the motor's rated torque at rated speed, not the stall torque (at 0 speed) which drops at higher speed due to spinning losses.

.