Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base VIDEO: How to import function blocks into ACR IEC_PLC projects
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base VIDEO: How to import function blocks into ACR IEC_PLC projects
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)-
        • Acrobasic commands for IEC PLC
        • ACRView 6.4.1 Runtime Error for 9600 and 9640
        • ACRView IEC Editor not Compatible with Win10
        • Converting ACR9600 Projects to ACR9000 Projects
        • General Function Block Behavior
        • How to add multiple outputs in ACR IEC PLC ladder programs
        • How to change the Task Type or Task Speed
        • How to change velocity on the fly
        • How to home to a limit in ACR96xx
        • How to Modify a ACR-View project (9600) AcroBasic only programs for Win10
        • How to run an AcroBasic program from IEC PLC
        • How to start the IEC PLC on controller power-up
        • How to use Direct Variable references in ACR IEC PLC
        • IEC Error Message: No valid license for the current hardware
        • Invert Motion Direction in IEC PLC
        • Is there a First Scan flag in the IEC PLC
        • PLCOpen State Machine
        • Set Compax3-EPL Current Limit
        • User Function Block : Excess Position Error Response
        • User Function Block : Moving Average
        • User Function Block : Rotary Axis Position
        • User Function Block: Read Actual Torque
        • User Function Block: Software Limits
        • Using arrays in IEC PLC
        • Using the IEC Debug Window and Watch Lists
        • Variable Declarations in IEC Languages
        • VIDEO: How to import function blocks into ACR IEC_PLC projects
        • What is a Moving Segment Error?
        • Why is the IEC PLC making the axis to move farther and faster than programmed?
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
VIDEO: How to import function blocks into ACR IEC_PLC projects

Print Friendly and PDF

21-Feb-2012  JW

Products: ACR9600, ACR9630, ACR9640

Re-using code is one of the biggest benefits of IEC61131 programming. Follow these simple steps to import a User Function Block into an ACR IEC project, or download and watch this video from more details.

 

Select either a LDD, ST or CFC file. The function block file will now be available for editing in the IEC PLC Browser. Double Click the file to edit, and Syntax Check complete the code.

 

After the file has been checked, it will be available for use within a Program or another user FB. Use either Insert Function Block or drag and drop from the IEC PLC Catalog/Project folder. If the FB is not shown in the Catalog, right click and select Refresh.

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply