Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Using ACR7xxx or ACR9xxx or IPA with LabView
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Using ACR7xxx or ACR9xxx or IPA with LabView
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
Using ACR7xxx or ACR9xxx or IPA with LabView

Print Friendly and PDF

Products: ACR9000,9030,9040,9600,9630,9640, AR-xxCE, Aries Controller, IPA

Parker Motion Manager (for ACR7000) and ACR-View 6 (for ACR9000, IPA and AriesController) includes a communication server, ComACRserver.exe for PC based applications. The ComACRserver library can be used in most programming environments that support COM objects, such as VB.Net, C++, C#, VB6 and LabView. The ComACRserver is installed with ACR-View in C:\Program Files\Parker\ACR-View 6 (default directory). ComACRserver User Guide

Sample LabView Project for ACR9000, Intelligent Parker Amplifier (IPA) or Aries Controller

The ComACRserver includes methods for setting and getting any bits or parameters on the ACR. These are efficient binary packets that can be set-up for regular polling or one time calls. Much of the ACR's functionaliity can be controlled via theses bits and parameters, including coordinated move commands. For functions that cannot be called this way, the ComACRserver includes a Terminal interface for sending Ascii commands.

It certainly possible to have an entire application controlled via the LabView interface, without any AcroBasic code running on controller. However in most applications, its often more practical to have code reside on the controller to be initiated from the user interface.

Additional Examples: two simple VI's  to initialize a connection with the com server and read or write, ACRserverRead, ACRserverWrite. The ACR_Connect VI is  used to issue a position command (set a p-parameter)  then read the actual position (read a p-parameter) back and plot it. 

Related FAQ:  PC to ACR Program Samples (Excel, LabView, VB.Net, C++, C#)   includes updated sample with writing to LabView

22-Feb-2012  jw

updated 08-Jul-2014 jw

update 17-Nov-2015 jw

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply