Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base ACR Binary Parameter Access Examples
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base ACR Binary Parameter Access Examples
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)-
        • Free Online Training Videos: Parker AcroBasic - Programming Basics
        • ACR7000 and ACR9000 Controller --- Interact Xpress HMI Jog Teach Sample
        • AcroBasic program does not wait
        • ACR Binary Parameter Access Examples
        • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
        • ACR Memory usage and commands
        • AcroBasic Program Priority and Timing
        • Axis Flag update rate
        • Change axis positive/negative motion direction
        • Clear all memory in an ACR controller
        • Command Syntax for Variable Substitution
        • Commenting AcroBASIC Programs
        • Concerns when using DWL in programs
        • Concerns when using INH in programs
        • Creating Watchdogs for Ethernet Connections
        • Encoder Velocity
        • Error 17000 when attempting to communicate to ACR
        • Evaluation Underflow error
        • Evaluation overflow is line xxx
        • Hardware Position Capture for Encoder 8 and 9
        • Homing Application Note for ACR7xxx/ACR9xxx Controllers and IPA Drives
        • How can I check the axis PPU setting?
        • How do I set the frequency in an ACR SINE move?
        • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
        • How fast is my servo axis moving?
        • How to Calculate the Gear Offset Parameter?
        • How to Find Torque or Current commanded from ACR
        • How to home to a limit in AcroBasic
        • How to receive ASCII data
        • How to retrieve the raw SSI position from encoder?
        • How to Simulate Motion (without drives or motors)?
        • How to use CAM ON when source is moving
        • How to use the In Motion Bit
        • INT command not working properly
        • INTCAP
        • Is the ComACRsrvr thread safe?
        • LISTEN / LRUN - How to see line numbers
        • Output on Position Toggle Mode
        • PID Parameters when using Steppers
        • Position to a Torque / Current Mode
        • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
        • prohibited names for Axis aliases
        • Range Error on download for IF ENDIF statements
        • Range Error when commanding long moves - Distance limit 2^31
        • Reboot in startup program
        • Stopping motion in ACR controllers
        • System Pointer Address of ACR Global Variables, P0-P4095
        • Use of AXIS format
        • User Variables
        • Using ACR7xxx or ACR9xxx or IPA with LabView
        • Using CAM with PPU in user units (not counts)
        • Using Encoder 8 or 9 as SRC
        • Using JOG commands with AXIS identifier
        • Using an encoder or analog input as JOG SRC
        • Variable data types and transfer to AB plc via Ethernet/IP
        • VB generates Runtime Error 91 (accessing through the ACR Comm Server)
        • What ACR Global variables should I use in HMI applications?
        • What is the Binary Host Interface
        • What is the axis velocity
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
ACR Binary Parameter Access Examples

Print Friendly and PDF

Supplement to ACR Programmers Guide,Binary Host Interface

Products: ACR9000,9030,9040,9600,9630,9640, AR-xxCE (Aries Controlller)

Binary parameter access provides a method of reading from and writing to single system parameters on the controller. Unlike binary data packets, binary parameter access uses the actual parameter number. There are no groups or masks.
A parameter access header consists of a Header ID ( 0x00 ) followed by a Packet ID code and a 2-byte parameter. The Packet ID codes for the different types of packets are shown below. The following pages define each of the packets in detail.

Packet ID Codes  
Code Packet Type Description
0x88 Binary Get Long Receive long integer from controller
0x89 Binary Set Long Send long integer to controller
0x8A Binary Get Float Receive Float value from controller
0x8B Binary Set Float Send Float value to controller

When using the Binary Parameter Access, the parameter is converted to hex. The parameter is a 2-byte value sent low-order byte first. Here are some examples:

P12288(current position, axis0) converts to 30 00. Request is sent to controller as 00 88 00 30
P12546(actual position, axis1) converts to 31 02. Request is sent to controller as 00 88 02 31
P8193(vector velocity) converts to 2001.  Request is sent to controller as 00 8A 01 20

 

VB.Net example for formatting the byte packets

Imports System.BitConverter

 

PublicFunction GetLongPacket(ByVal iParm AsInteger) As System.Array
Dim bArr(3) As Byte
Dim byteParm(1) As Byte
bArr(0) = &H0
bArr(1) = &H88
byteParm = BitConverter.GetBytes(iParm)
System.Array.Copy(byteParm, 0, bArr, 2, 2)
Return  bArr
End Function
 
 

23-Mar-2012

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply