22-Feb-2012
Products: ACR9600,9630,9640, ACR-View, IEC PLC
It is possible to have multiple outputs(parallel coils) in ACR-View IEC PLC Ladder programs. Click on the rung in front of the coil, then either right click (figure2) and select insert coil or use the coil icon in the menu bar(figure1).