Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Dual Loop with Analog Position Feedback
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Dual Loop with Analog Position Feedback
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
  • -Motion and Machine Controllers
    • -ACR Controllers
      • +7000
      • -9000 (Legacy)
        • ACR9000 Family Letter of Volatility
        • ACR Gantry Lock and EPL Axes
        • ACR Homing Success/Failure Flags
        • ACR Order Code
        • ACR Servo Tuner - Move Back & Forth sample code
        • ACR-View 6 is frozen. How do I recover?
        • ACR-View Memory Dimensioning using the Oscilloscope
        • ACR9000 to ModuFlex connection pinout
        • Automating the EPL startup procedure
        • Can I use tools from ACR-View in my own PC application?
        • Compax3 and Aries Ethernet PowerLink I/O
        • Configuring Memory for ACR9000 Com Channels
        • Dual Loop with Analog Position Feedback
        • EPL Drive Enable Status
        • Free Online Training Videos: Parker ACR9000 programmable motion controller
        • Having problems connecting with USB - ACR View 6.0
        • How do I add PBOOT to PLC programs?
        • How much memory does my ACR controller have?
        • How to Read Compax3 Analog I/O with EPL SDO read?
        • How to connect ACR to PIO CANopen buscoupler?
        • How to disable RS232 autobaud for ACR9xxx
        • How to get status values from an Aries EPL Drive
        • How to read the absolute position from EPL drive?
        • How to select user units and axis scaling
        • INTCAP and MSEEK with Compax3 EPL
        • MSEEK EthernetPowerlink Compatibility
        • Memory Allocation for PLC programs
        • Output Reaction to EPL Failure
        • Remap CAN I/O for use with PLC
        • What is needed with various Parker I/Os?
        • What verison of the .Net Framework is needed for ACR-View 6?
        • Whats the difference between PIO-337 and PIO-347?
        • Where does ACR-View install the ComACRserver?
        • Why is controller reporting Program Stuck
        • 9000: Connector Part Numbers
        • ACR 9000 replacement: New ACR7000 series controller
        • ACR 9xx0 Recovering from Estop / Motion Enable input
        • ACR-View: Mapping a parameter to an oscilloscope channel
        • ACR9000 - CIP Communications stop on all devices when one CIP device goes offline
        • ACR9000 Ethernet Stream Connection Status Sample
        • ACR9000 Event Counters
        • ACR9000 Sample Input/Output Wiring
        • Are Parker IO modules available as NPN?
        • Connecting a Parker IO (PIO) to an ACR9000
        • EPL Velocity p38145 vs p8193 Master Velocity
        • Ethernet Communication Streams
        • Ethernet/IP Encoders
        • How do I set up Parker I/O (PIO)
        • How to command a home operation from HMI or PC app
        • Master Encoder for C3 EPL & ACR9040 system
        • Maximum USB Cable Length
        • Replacing the ACR9000 Battery
        • RS232 Electrical Noise on older 9000 Controllers
        • Senary Axis Flags
        • Updated EPL Network Flags and Parameters
        • Upload Absolute Position from a C3 to a ACR9000
      • +IEC PLC (9600) (Legacy)
      • +PC Card Controllers (Discontinued)
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • +PAC120
    • +PAC340
    • +PAC320 (Discontinued)
    • +6K (Discontinued)
  • +General Technology Information
  • +Virtual Engineer
  • +Visualization and Human Machine Interface (HMI)
  • +Servo Drives and Servo Drive/Controllers
  • +Stepper Drives and Stepper Drive/Controller
  • +Gearheads
  • +AC and DC Drives and Inverters
  • +Servo Motors
  • +Step Motors
  • +Linear and Rotary Positioners
  • +Electric Cylinders
  • +T-Slot Aluminum Framing
  • +C3 + Xpress + ETH
  • How can I stay updated on Parker electromechanical and drives product news?
  • +Legacy (Discontinued)
  • +Other
  • Memorandum: Information on EPA ban of Persistent bioaccumulative toxin (PBT)
  • What replaces the Gemini GV6K servo drive controller?

You are currently reviewing an older revision of this page.

  • History View current version

Dual Loop with Analog Position Feedback

By default, each encoder and DAC is set to the same index as the axis to which it is attached (for example, ATTACH AXIS0 ENC0 DAC0 ENC0). It is good programming practice to use the same index for the feedback or signal output as the axis to which you are attaching.
For example, to attach ADC 4 as position feedback, and DAC 4 as the command signal to axis 4, send the following:
ATTACH AXIS4 ADC4 DAC4 ADC4
 
There is one exception: dual-loop feedback. With dual-loop feedback, you can attach a second feedback source to an axis. In this case, you must indicate which additional encoder is being used.
For example, to attach encoder 4 as position feedback, DAC 4 as the command signal, and encoder 9 as the velocity feedback, send the following:
ATTACH AXIS4 ENC4 DAC4 ENC9
 
So for dual loop, you could use the analog sensor feedback for position and use the encoder feedback for the velocity:
ATTACH AXIS4 ADC4 DAC4 ENC4
 
You can use the same ADC and ENC on the same axis so you don't have to use an extra axis just as ADC input.  Only thing with this last dual loop code, you can only monitor the ADC position, not the velocity, and only monitor the encoder velocity but that should be fine for most applications.
 
One example of analog position feedback sensor's includes MTS Sensor Corp's Linear Sensors:
http://www.mtssensors.com/

 

For an even better designed system, the ACR9000 axis connector supports SSI feedback which is a digital transmission instead of analog. This is a standard option from MTS Sensor and most other manufacturers and is configured the same as the analog above. The SSI feedback is better for industrial installations and it's feedback cannot be corrupted by EMI noise.