Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base What is a Moving Segment Error?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base What is a Moving Segment Error?
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)-
        • Acrobasic commands for IEC PLC
        • ACRView 6.4.1 Runtime Error for 9600 and 9640
        • ACRView IEC Editor not Compatible with Win10
        • Converting ACR9600 Projects to ACR9000 Projects
        • General Function Block Behavior
        • How to add multiple outputs in ACR IEC PLC ladder programs
        • How to change the Task Type or Task Speed
        • How to change velocity on the fly
        • How to home to a limit in ACR96xx
        • How to Modify a ACR-View project (9600) AcroBasic only programs for Win10
        • How to run an AcroBasic program from IEC PLC
        • How to start the IEC PLC on controller power-up
        • How to use Direct Variable references in ACR IEC PLC
        • IEC Error Message: No valid license for the current hardware
        • Invert Motion Direction in IEC PLC
        • Is there a First Scan flag in the IEC PLC
        • PLCOpen State Machine
        • Set Compax3-EPL Current Limit
        • User Function Block : Excess Position Error Response
        • User Function Block : Moving Average
        • User Function Block : Rotary Axis Position
        • User Function Block: Read Actual Torque
        • User Function Block: Software Limits
        • Using arrays in IEC PLC
        • Using the IEC Debug Window and Watch Lists
        • Variable Declarations in IEC Languages
        • VIDEO: How to import function blocks into ACR IEC_PLC projects
        • What is a Moving Segment Error?
        • Why is the IEC PLC making the axis to move farther and faster than programmed?
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
What is a Moving Segment Error?

Print Friendly and PDF
Products: ACR9600, 9630,9640
Moving Segment Error
When loading a Program to the PLC by going online, you may get the Error message:
 
Loading the program will be aborted. You will still be online with the PLC, so "upload error log"

This will place a txt file in the PLC Brower:

 

 

Open the file to see the error:
 
Possible errors:
Error ID
Message
Reason
Example
1
ACR flag range error Flag:
flag number does not exist on ACR
MyBool : Bool AT%B99999
2
ACR flag drive I/O Flag:
drive I/o flags
MyBool : Bool AT%BW70
3
ACR flag drive I/O Flag:
Restricted Flags (see list below)
MyBool : Bool AT%BW8468
4
ACR parameter not dimensioned Parameter:
Global Vars not dimensioned
MyReal : REAL AT%P200;
5
ACR parameter range error Parameter:
parameter number does not exist on ACR
MyReal : REAL AT%P99900
 
The following flags CANNOT BE ASSIGNED AS AT%BW (read/write), a Moving Segment Error will result.
These bits can still get set thru the PLC, using MC_WriteBoolParameter or ACR_WriteFlag
 
 
Bit Range
Desc
ErrorID
768
1023
Primary Axis Flags (Axes 0-7)
3
7680
7935
Primary Axis Flags (Axes 8-15)
3
512
767
Primary Master Flags (Masters 0-7)
3
40
47
Drive Enable Outputs
2
48
55
Drive Reset Outputs
2
56
63
LEDs
2
64
71
Drive Fault Inputs
2
96
103
LEDs
2
112
115
Trigger captures
3
 
 
 

 

 

 

 

 

JW 2012

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply