Old Unit | Replaced By | Software Required | Notes |
P11/PMP/P1H 6" QVGA 320x240 |
P1306QT-Q3 | Interact 7 (Windows XP) | For Class 1 Div 2, replace ending 3 with 5 |
P12-3## 6" QVGA 320x240 |
P1306QT-Q3 | Interact 7 (Windows XP) | For Class 1 Div 2, replace ending 3 with 5 |
P12-4## 6" VGA 640x480 |
P1306VT-Q3 | Interact 7 (Windows XP) | For Class 1 Div 2, replace ending 3 with 5 |
Information on the P13 Family can be found at the following link:
http://www.parkermotion.com/products/Dedicated_HMI__5937__30_32_80_567_29.html
Old Unit | Replaced By | Software Required | Notes |
P15/P2x/P3x/P4x/P5x/PS10/PA10 | PA210T-133 | Interact 7 (Windows XP) | For Class 1 Div 2, replace ending 3 with 5 |
PA06S (PA05S - no 5" units) | PA206Q-133 | Interact 7 (Windows XP) | For Class 1 Div 2, replace ending 3 with 5 |
PA08S | PA208T-133 | Interact 7 (Windows XP) | For Class 1 Div 2, replace ending 3 with 5 |
PA15T/PS15 | PA215T-133 | Interact 7 (Windows XP) | For Class 1 Div 2, replace ending 3 with 5 |
Information on the PA2 Family can be found at the following link:
http://www.parkermotion.com/products/Dedicated_HMI__7292__30_32_80_567_29.html
Keep in mind the following BEFORE ordering a new unit.
1. The PA2 and P13 series do not support PC104/ISA bus cards. If you are using these, please re-evaluate the application.
2. The PA2 and P13 series ONLY has 2 serial ports. If you are using more than 2 serial connections or printing from LPT1, please re-evaluate the application.
We no longer manufacture hardware with 3 com ports or Parallel Printer Ports that can run MSDOS Interact Runtime.
3. Interact Software upgrade is REQUIRED. Interact Software is only compatible with Windows XP and will not work in Window 7 XP Mode.
4. Interact software is an additional purchase.
Interact:
- PA2 units are pre-loaded with (and require) Interact7 runtime.
- ALL optional runtime modules are included with every PA2. With older versions of Powerstations like the PA, runtime modules were selected with additional cost to the hardware.
- PA2s can run projects developed in older versions of Interact, but must first be upgraded using Interact 7
- Interact 7 Development software Part numbers:
Model # Description MSP-7NA0-P Interact7 Development (new user) IUP-6070-6 Interact Development Upgrade to 7.X from 6.X IUP-6070-5 Interact Development Upgrade to 7.X from 5.X
Last Modified 3/27/2012 by KJAX
edited dom 07/24/2019