Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base ACR Memory usage and commands
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base ACR Memory usage and commands
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
ACR Memory usage and commands

Print Friendly and PDF

See also : User Variables

AcroBASIC Command

9000/9030/9040

Aries CE Controller

FLASH ERASE

Erases the user image from flash

Erases stored programs

FLASH LOAD

Loads the user image from flash.

Loads programs from flash

FLASH RES

Command returns the controller to factory settings. Performs the following actions:

  • clears all memory dimensioned for programs, variable, arrays, and data logging
  •  resets the communication stream dimensions
  •   erases all system parameters
  •  erases user images from flash memory
  •   resets the hardware configuration
  •   cycles power to the controller.

Command returns the controller to factory settings.

Performs the following actions:

Erases motor configuration and user programs (ERASE + FLASH ERASE)

FLASH SAVE

Stores an image of the user programs and PLC programs in the flash.

If the image is detected in the flash on power-up, the card will load user programs and PLC†s from flash instead of relying on the battery backup memory. User Global Variables reside in battery backup memory and are not affected by the program transfer.

Saves all programs to flash

FLASH IMAGE

stores an image of the user programs and PLC programs, as well as the User Global Variables

If an image is detected in the flash on power-up, the controller loads the user programs, PLCs, and user variables from flash instead of relying on the battery backup memory.

Saves all programs to flash

ESAVE

stores system parameters into flash system parameter section to be retrieved on power-up or by issuing an ELOAD command

N/A

ERASE

erases all system parameter information from the flash system parameter. When you next cycle power, the controller uses the factory default settings or flash values.

NOTE: This command should be used with caution since it destroys setup information.

NOTE: returns IP address back to default.

NOTE: Program memory allocation is stored in battery-backup RAM, not in the EEPROM.

NOTE: FLASH commands (FLASH SAVE, FLASH ERASE, etc.) have no effect on the system parameters.

 

 

 

 

 

Erases motor configuration parameters and drive setup parameters and sets them to their defaults. Does not erase stored programs

 

Erased drive and axis parameters

 

Reboots controller

 

 

 

 

 

90x0PxUxMx

90x0PxUxBx

AR-xxCE

Save User Programs

 

FLASH SAVE or FLASH IMAGE

Programs retained in USER RAM with BBRAM

FLASH SAVE or FLASH IMAGE

Save System Parameters

(Attachments, Masters)

ESAVE

ESAVE

FLASH SAVE or FLASH IMAGE

Clear User Programs

 

FLASH ERASE

NEW or NEW ALL

FLASH ERASE

Save Axis Set-up  Parameters

(Gains, PPU, etc)

ESAVE

ESAVE

Retained in Non-Volatile USER RAM

Save Local Variables and Arrays

N/R*

Retained in USER RAM with BBRAM

Retained in Non-Volatile USER RAM

Save User Global Double Variables

P0 - P4095

FLASH IMAGE

Retained in USER RAM with BBRAM

FLASH IMAGE

Save User Global Single Variables**

P39168 - P39423

N/R*

Retained in USER RAM with BBRAM

P39168-39231 retained  in Non-volatile User RAM  

Save User Global Long Variables**

P38912 - P39167

N/R*

Retained in USER RAM with BBRAM

P38912-38975 retained  in Non-volatile User RAM  

 

* N/R = Not retained after power cycle

**Requires OS revision 1.24 for ACR90x0, OS revision 1.13 for AR-CE.  These variables do not require dimensioning prior to use.