Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base AcroBasic Program Priority and Timing
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base AcroBasic Program Priority and Timing
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)+
      • PC Card Controllers (Discontinued)+
      • ACR Binary Parameter Access Examples
      • ACR Controllers: Excel Spreadsheet Example for ACR and IPA
      • ACR Memory usage and commands
      • AcroBasic Program Priority and Timing
      • AcroBasic program does not wait
      • Change axis positive/negative motion direction
      • Clear all memory in an ACR controller
      • Command Syntax for Variable Substitution
      • Commenting AcroBASIC Programs
      • Concerns when using DWL in programs
      • Concerns when using INH in programs
      • Creating Watchdogs for Ethernet Connections
      • Encoder Velocity
      • Error 17000 when attempting to communicate to ACR
      • Evaluation Underflow error
      • Evaluation overflow is line xxx
      • Free Online Training Videos: Parker AcroBasic - Programming Basics
      • Hardware Position Capture for Encoder 8 and 9
      • Homing Application note for ACR9xxx controllers
      • How can I check the axis PPU setting?
      • How do I set the frequency in an ACR SINE move?
      • How does motion work in the ACR products (ACR7xxx, ACR9xxx, IPA, Aries-CE)
      • How fast is my servo axis moving?
      • How to Calculate the Gear Offset Parameter?
      • How to Find Torque or Current commanded from ACR
      • How to Simulate Motion (without drives or motors)?
      • How to home to a limit in AcroBasic
      • How to receive ASCII data
      • How to retrieve the raw SSI position from encoder?
      • How to use CAM ON when source is moving
      • How to use the In Motion Bit
      • INT command not working properly
      • INTCAP
      • Is the ComACRsrvr thread safe?
      • LISTEN / LRUN - How to see line numbers
      • MFLOPS vs. MIPS
      • Output on Position Toggle Mode
      • PID Parameters when using Steppers
      • Position to a Torque / Current Mode
      • Programmable Limit Switch (PLS) feature in the ACR9xxx and IPA
      • prohibited names for Axis aliases
      • Range Error on download for IF ENDIF statements
      • Reboot in startup program
      • Stopping motion in ACR controllers
      • System Pointer Address of ACR Global Variables, P0-P4095
      • Use of AXIS format
      • User Variables
      • Using ACR9xxx or IPA with LabView
      • Using CAM with PPU in user units (not counts)
      • Using Encoder 8 or 9 as SRC
      • Using JOG commands with AXIS identifier
      • Using an encoder or analog input as JOG SRC
      • VB generates Runtime Error 91
      • Variable data types and transfer to AB plc via Ethernet/IP
      • What ACR Global variables should I use in HMI applications?
      • What is the Binary Host Interface
      • What is the axis velocity
      • How to Wire Limit Sensors to ACR9xxx and ACR7000 Controller
      • ACR7000 Controller and ACR9000 Xpress Jog Teach Sample
      • Axis Flag update rate
      • Range Error when commanding long moves - Distance limit 2^31
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
AcroBasic Program Priority and Timing

Print Friendly and PDF

Products: ACR9000, 9030,9040,9600,9630,9640, Aries CE, IPA

16 AcroBasic programs are available for use in ACR controllers.  In the ACR9xxx's and IPA, Programs 0-7 are high priority and 8-15 are low priority. In the AriesCE Program 0 is high priority, 1-15 are low priority.

Controller Type
High Priority Programs
Low Priority 
Programs
IPA
  0 - 7
  8 - 15
ACR9xxx(all variants)
  0 - 7
  8 - 15
Aries Controller
  0
  1 - 15  

High priority programs each have a dedicated time slice, where the low priority programs share a time slice. Communications also have a dedicated high priority task. Each time slice is 1ms, within that time the programs will execute anywhere from 1-10 lines of code before switching to the next program in the queue.

An example of the operation order where 0-9 are all being used would proceed as follows:

0,1,2,3,4,5,6,7,COM,8
0,1,2,3,4,5,6,7,COM,9
0,1,2,3,4,5,6,7,COM,8
 
Notes:
  • Programs will only utilize their time slices when they are actually running.
  • The program priorities are fixed in the controller, there is no provision for adjusting the priorities for the user. 
  • DWL statements in low priority programs will cause the entire low priority slice to DWL
  • INH statements in low priority programs will inhibit the entire low priority slice
  • PROG15 is used by the ACR-View to store the configuration. Users should avoid using this program for other purposes.


edit 6-jan-2016  jw...add ipa