Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Compax3 Training - C3ServoManager - How to Create Custom Rotary Motor File (Video)
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Compax3 Training - C3ServoManager - How to Create Custom Rotary Motor File (Video)
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3-
      • Compax3 Accessories - BDM restrictions
      • Compax3 Accessories - BDM Editing Move Profile Table for T11
      • Compax3 Accessories - BDM01/01 Keypad Capability
      • Compax3 Accessories - BRM Braking Resistor Information
      • Compax3 Accessories - MDR Motor Choke Specification Sheets
      • Compax3 Accessories - VM15 Breakout Modules (15pin Connectors Genders)
      • Compax3 Accessories - What Does the PIO_Init Device Input Refer To?
      • Compax3 Cables - MOK Motor Power and GBK or REK Feedback Cables
      • Compax3 Misc - ASCII Serial Communications (with Examples)
      • Compax3 Misc - C3-MotorManager Setting the Beginning and End of Saturation Values
      • Compax3 Accessories - Expansion I/O (PIO) with the Compax3?
      • Compax3 Accessories - NFI Line Filter Specification Sheets
      • Compax3 Accessories - PS or Option 5 wiring option to Compax3
      • Compax3 Misc - CTC HMI's to Compax3 Options and Wiring
      • Compax3 Hardware - Can I Run My Compax3 V4 with Single Phase VAC?
      • Compax3 Hardware - Can the Compax and Compax3 Products take a DC voltage supply?
      • Compax3 Hardware - Can the Compax3 be Used at 24volts? Or Other DC Voltages? Or 120VAC?
      • Compax3 Hardware - Can the Compax3 Drives Share the DC Bus Connection?
      • Compax3 Hardware - 24 Volt Step & Direction Inputs (Pulldown Resistor May be Needed)
      • Compax3 Hardware - BRM Braking Resistor Specifications
      • Compax3 Hardware - C3H Communications Ports
      • Compax3 Hardware - Can the Compax3 generate a Z pulse when using resolver feedback?
      • Compax3 Hardware - Compax3M Servo Drive/Controller STO not offered
      • Compax3 Hardware - Connector Part Numbers
      • Compax3 Hardware - Convert F10 / F12, M12 additional IO, Convert Fieldbus I20, I21, I22, I30, I31
      • Compax3 Hardware - Inrush Current
      • Compax3 Hardware - EnDat 2.2 Compatible
      • Compax3 Hardware - MaxPlus (MPM) Option 1 Brake Connection
      • Compax3 MaxPlus (MPM) Encoder Option 1 Connection
      • Compax3 MaxPlus (MPM) Resolver Option 1 Connection
      • Compax3 Hardware - Wiring for Apex Motors and Motor Files
      • Compax3 Hardware - What are the input & output functions on the C3 x11 x12 and x22 connectors?
      • Compax3 Hardware - What are the minimum connections for an I10 T10?
      • Compax3 Hardware - What are the voltage specifications for the analog inputs?
      • Compax3 Hardware - What is the Compax3 resolver frequency (X13)?
      • Compax3 Hardware - X11 Connector
      • Compax3 Misc - Absolute Encoder Compatibility (EnDat and Hyperface)
      • Compax3 Misc - Auto-commutation (Hall-less Commutation)
      • Compax3 Misc - Brake Delay/Engage Settings
      • Compax3 Misc - Can a MX80L be Used?
      • Compax3 Misc - Can I Perform Gearing on the I10T10?
      • Compax3 Misc - C3F Support
      • Compax3 Misc - Changing Gear Ratio on the Fly with the T11
      • Compax3 Misc - Compax3 EtherCAT Delta robot (Video)
      • Compax3 Misc - Connecting an ACM2n Motor
      • Compax3 Misc - EMC Compliance
      • Compax3 Misc - EPL Dual Loop Configuration with ACR9040-EPL Controller
      • Compax3 Misc - EtherCat Compatible Controllers (for I31 EtherCAT Option)
      • Compax3 Misc - F11 Stegmann SinCos Hyperface encoder option replaced by F10 option
      • Compax3 Misc - Homing a SinCos System
      • Compax3 Misc - How to Set C3 to Xpress with RS485 4-wire / RS422
      • Compax3 Misc - Homing in a T11
      • Compax3 Misc - How do I jog or home using a Compax3 I20T11?
      • Compax3 Misc - I10T10 jogging & position in the Optimization Tool
      • Compax3 Misc - I12T11 or I11T11 Differences
      • Compax3 Misc - Letter of Volatility (All Models)
      • Compax3 Misc - Model Numbers Explained (Input, Technology and Control Options - IxxTxxMxx)
      • Compax3 Misc - Positioning to Machine Zero After Homing and Machine Zero Offset
      • Compax3 Misc - Profibus (I20) vs. Digital I/O (I11)
      • Compax3 Misc - Using R100D, R150D, R200D with Compax3
      • Compax3 Misc - What are the general requirements for supported SSI feedbacks?
      • Compax3 Software - Accessing Objects from RS232 and RS485
      • Compax3 Software - Are There Separate Proportional and Integral Gain Settings?
      • Compax3 Software - C3ServoManager - Motor Database Update (7D encoders)
      • Compax3 Software - Communicating to the Compax3 I12T11 Indexer from a Panasonic PLC over DeviceNet
      • Compax3 Software - Commutation Operation (F12)
      • Compax3 Software - Firmware and C3ServoManager Archive
      • Compax3 Software - Gearing Setup on a T11 and T40
      • Compax3 Software - Homing Mode Changes After Configuration
      • Compax3 Software - How do I set current (torque) limiting?
      • Compax3 Software - How do I setup scaling in a Compax3?
      • Compax3 Software - How to Change C3 Torque Limit via EPL (SDO Write)
      • Compax3 Software - How to get status values from an C3 EPL Drive (I30)
      • Compax3 Software - T30/T40 - C3_Input and C3_Output function blocks need EN enable in Ladder
      • Compax3 Software - T30/T40 - Example of Using the D to A Monitors
      • Compax3 Software - T30/T40 - Getting Actual Torque / Current Values
      • Compax3 Software - T30/T40 - How do I add C3 IEC library? How do I install/change targets? 5830 3740 errors
      • Compax3 Software - T30/T40 - How Do I Use the FOR Loop?
      • Compax3 Software - T30/T40 - IEC Programming Tips and Code Examples
      • Compax3 Software - T30/T40 - Convert Integer to Binary Pattern - Useful IEC Functions (Examples)
      • Compax3 Software - T30/T40 - Necessary Codesys components for T30/T40 and C3ServoManager
      • Compax3 Software - T30/T40 - Useful IEC Function Examples (Convert Binary Pattern to Integer)
      • Compax3 Software - T30/T40 - Useful IEC Function Examples (Moving/Not Moving Signal)
      • Compax3 Software - T30/T40 - Useful IEC Function Examples (Reset - Enable - Home Function Blocks)
      • Compax3 Software - C3ServoManager - How to Export Oscilloscope Data to .csv
      • Compax3 Software - C3ServoManager - How to View or Monitor any Object in Optimization (Activate Object Tree)
      • Compax3 Software - How to completely clear (factory default) the Compax3
      • Compax3 Software - What is a GSD and EDS File and Where Can I Download Them?
      • Compax3 Training - I10T10 Training Videos
      • Compax3 Training - Navigating Codesys Quick Tips
      • Compax3 Hardware - RS485: PC connections through B&B Electronics 485BAT3 to C3
      • Compax3 Software - T30/T40 - Useful IEC Function Examples (Read Analog Inputs)
      • Compax3 Troubleshooting - Recover from Tracking Error Fault
      • Compax3 Misc - Reset Absolute Encoder Position - Store In Drive or Motor?
      • Compax3 Misc - SSI signal source for the Compax3
      • Compax3 Software - How to Save to Flash through RS-232/485
      • Compax3 Software - C3ServoManager - Saving Help Files During Upgrade or Reinstall.
      • Compax3 Hardware - Simulated Encoder Output (X11)
      • Compax3 Hardware - Single Ended Step & Direction (I10T10
      • Compax3 Misc - Single Turn Absolute Encoder - Position always 0 on power-up?
      • Compax3 Misc - T11 Positioning Profiles
      • Compax3 Software - T30/T40 - Where is the Analog Inputs Status?
      • Compax3 Software - TCP/IP via EPL Hardware (I30)
      • Compax3 Software - T30/T40 - Useful IEC Function Examples (Toggle Function)
      • Compax3 Software - T30/T40 - Useful IEC Function Examples (Torque Control Sample with Interact Xpress Panels)
      • Compax3 Software - C3ServoManager - Troubleshooting the Inertia Calculator (Auto Inertia Detection)
      • Compax3 Misc - TwinCAT Setting - Change Sync Shift Time from default
      • Compax3 Misc - Why are There Two labels on Compax3 (A90 on label)?
      • Compax3 Training - How do I tune (auto-tune) a Compax3? (Video)
      • Compax3 Training - I11T11 Training Videos
      • Compax3 Training - I11T30 Training Videos
      • Compax3 Training - Analog Velocity / Joystick program for Compax3 (Video)
      • Compax3 Training - Analog position / Joystick program for Compax3 (Video)
      • Compax3 Training- C3ServoManager - How to Tune Linear Servo with the Compax3 (Video)
      • Compax3 Training - Direct Drive Motors with Ethernet Powerlink Drives (I30) (Video)
      • Compax3 Training - C3ServoManager - How to Create Custom Linear Motor File for Compax3 (Video)
      • Compax3 Training - C3ServoManager - How to Create Custom Rotary Motor File (Video)
      • Compax3 Training - How to configure Compax3 I31T11 EtherCAT (Video)
      • Compax3 Software - T30/T40 - Example Program: Life Test Cycle (Video)
      • Compax3 Hardware - What are the minimum connections for an I12 T11?
      • Compax3 Training - Interact Xpress HMI to Compax3 T30 Sample Project (VIDEO)
      • Compax3 Troubleshooting - BDM Display shows "Load Menue!"
      • Compax3 Troubleshooting - C3ServoManager - Error Trying to Launch Codesys: "The parameter is not correct."
      • Compax3 Troubleshooting - Can't View Compax3 Help Files (chm)
      • Compax3 Troubleshooting - Cannot Communicate via RS232 Serial (C3 ServoManager or Other Software)
      • Compax3 Troubleshooting - Codesys Error 5827 #1027 Unknown Command
      • Compax3 Troubleshooting - Codesys Error 5830 #1030 Invalid Operand EQ Axis Ref Fieldbus
      • Compax3 Troubleshooting - Codesys Error 5846 #1046 too many 16bit variables
      • Compax3 Troubleshooting - Codesys Error 5847 #1047 too many 32bit variables
      • Compax3 Troubleshooting - Compax3M Troubleshooting Tips for Communications
      • Compax3 Troubleshooting - C3ServoManager - Where is my motor file?
      • Compax3 Troubleshooting - Error History
      • Compax3 Troubleshooting - Error List
      • Compax3 Troubleshooting - Error When Installing C3 ServoManager on Windows 10
      • Compax3 Troubleshooting - Feedback Resolver Too Low (Fault 0x7382)
      • Compax3 Troubleshooting - How to find the error code for a Compax3 EPL drive (I30)
      • Compax3 Troubleshooting - I12 Inputs Not Working
      • Compax3 Troubleshooting - No Motion on a I12T11 with RS232/485 Control
      • Compax3 Troubleshooting - Red Light Fault (How Do I See What the Fault Is?)
      • Compax3 Software - Remanent Variables - VAR RETAIN
      • Compax3 Software - T30/T40 - Link versus Import Codesys 61131 project
      • Compax3 Training - Basics: How to Upload & Download (Video)
      • CRC = FFFF CAM no source package loaded
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
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
Compax3 Training - C3ServoManager - How to Create Custom Rotary Motor File (Video)

Print Friendly and PDF

How to create custom servo motor files for the Compax3 using the C3 ServoManager software's MotorManager

This is a 4 part video explaining how to use the Parker Compax3's C3 ServoManager software to create custom motor files for rotary motors. Explains parker North America custom rotary servo motor part numbering. Shows creating the file, automatic setting of commutation parameters, which feedback types are supported on the different Compax3 F10, F11, F12, and then a quick functional test of configuring the drive and jogging the motor in the Optimization screen.

MOBILE USERS CLICK HERE

Part 1: Connecting to the Compax3, Starting the Motor Manager, Overview of the structure of the Motor Manager

 

Part 2: Part Numbering for standard and custom Parker Electromechanical NA rotary servo motors

 

Part 3: Creating the custom rotary servo motor file

 

Part 4: Automatic setting of commutation parameters, Quick drive configuration and jogging from Optimization screen, How to email (.c3p includes motor file, or .xml Export & Import)

 

10/1/12jh

 

 

Hello. Today I'll be demonstrating how to create a rotary servo motor file for the Compax3 using the C3 ServoManager software.

The C3 ServoManager has libraries for most standard Parker motors.

This process can be used for any custom rotary motors or for machines with existing non-Parker motors where the Compax3 is now being integrated.

 
The software makes it easy to do this but there are a lot of steps involved so this video will help explain the steps and options.

 
I'll assume you have your Compax3's 24vdc control powered on as well as the AC power.

The Compax3S and Compax3M's safe torque off input and enable inputs are powered.

The motor and optional brake is connected to the x3 and the feedback to the x13.

 
We'll be controlling it through the software so the inputs and outputs on the x11 and x12 and optional x22 connectors do not need to be wired.

 
For a custom motor file it would be best if it is not connected to the load.

The automatic setting of commutation parameters will detect the feedback angle and frictional & large inertial loads could cause problems so if you can disconnect the motor from the load, that would be best.

 
It'll just spin the motor so if you want to disconnect the coupling and load from the motor shaft and/or put the motor on the floor, it shouldn't be doing any high speed or accelerations.

It would only do this with a bad feedback cable and mostly like would trip on a feedback fault but in the event, keep anyone away from the motor.

 
First, go to Options > RS232/485 com port settings.

You can see which COM ports available. You may need to go into your PC's DeviceManager to see which PORT you are connected to. Then in the main screen, click the Open/Close Com Port icon.

You should see in the status bar the port open.

You can verify on the top left > open Device selection and double-clicking Online Device Identification

This will connect to the drive and show the Device Type, what the Compax3 is configured as,

the firmware release number, controller board hardware level.

 
If you need the existing drive configuration, we'll be overwriting it today so upload and save the drive configuration.

Then create a new one by File > New.

 
Second go into Edit > Start C3-Motor Manager or from the tool bar, click on the Motor icon.

 
The MotorManager has two main parts,

the Motor library which has all the pre-defined Parker motors.

These are divided by both Rotary and Linear motors.

Those are then further categorized based on the feedback type:

Resolver, SinCos (Stegmann Hyperface), Endat (Heidenhain) Encoder (incremental)

Then based on Parker Europe or Parker US.

 
Down below, you have Edit Motor library.

You can create your own rotary motor file or linear servo motor file.

 
 
You'll need the full specifications of the servo motor to create these files.

 
If it's a custom Parker motor from Parker Electromechanical North America, unless it's

a ground-up custom, most of our custom motors are modified versions of our standard

servo motors.

 
Custom rotary servo motor part numbers are different formats depending upon

the age and the standard motor it is based upon:

 
CM233AE-115500 would be a custom SM233AE motor. The -115500 is a 6-digit incremental

number. This format custom part number is used for SM, BE, NeoMetric/J series servo

motors and use a 5digit or 6 digit number suffix. (You can tell if it's a BE23 versus

a SM23 motor based upon the winding letter. The SM motor has the A and B windings. The

BE uses the D, F, G, H,K, L, J windings.) You could also look at the motor, the SM is housed

where the BE is stamped lam.

 
Custom MPP and MPJ motors begin with CMP and CMJ.

 
Similar to the above format with the frame, stack length, winding, feedback and

6digit incremental number (begins at 200000).

ie, CMP0922R41-200827 is a custom MPP, 92mm frame, 2 stack length, 41 resolver.

CMP921B7D-200800

CMJ1426B6S-200802

 
Newer custom MPM motors begin with MPC, such as MPC1422B-115713 would be a custom MPM,

142mm frame, 2 stack length, B winding.

 
Older MPM custom motors end in 3 or 4 digit sequential number. ie MPM664-623 is a custom

MPM motor, 66mm frame, 4 stack length. If this is on an existing machine, you may contact

the machine builder for motor specifications or the factory. These part numbers do not

indicate the winding but the label on the side of the motor should give the resistance

and inductance and if it's a standard it'd be the same as what's in the motor manager.

 
 
Other than the older MPM, If it's a non-standard winding, it will be an X where the winding letter should be (ie, CM233XE would be a custom motor with non-standard winding). If it's a non-standard

feedback, it would be an X (ie, CM233AX would be a custom SM233 motor with A winding

and non-standard feedback). Presuming this is a new motor, you should have received the

specifications from your Parker Automation Technology Center distributor with the current,

resistance, inductance, rated speed, etc. If you don't have those, you may contact your ATC.

 
If it's an existing motor and a non-standard winding,

if it's proprietary motor, you'll need to contact the machine builder for those specifications.

If you're not sure if it's proprietary or not, you can contact the factory or your local ATC.

To contact the Parker North America, you can email emn.service@support.parker.com

For any Parker Europe motors, you can email parker.germany@parker.com

 
 
Assuming the motor is a modified standard, you can find the standard motor it's based on and use

it as a template. Right click from the Motor Library or Edit Motor Library, double-click on template.

 
If this is a non-parker motor, under Edit Motor Library, double-click on New.

 
Step 1, you can name your motor. These will appear under User Defined motors instead of Parker US or Parker Europe motors.

You can also add a comment for this file.

Each type you Use as template it'll always set the name as Copy As then the motor part number.

If you do multiple motor files, it'll always have the same name. The last one created is on the top of the list.

If you ever connect to another drive and do an upload, it'll import that motor file if it's custom motor file.

You can look at the summary screen to see the differences but in the drive configuration it'd be difficult to determine which is correct so it's good practice to re-name it.

 
Step 2 has the motor's pole count, the motor voltage constant. This says Volts/1000rpm and it is the peak of the sine wave.

Rotary inertia is set in kg-mm2

The continuous stall current is at 0 speed, is in Arms and in milliamps.

The peak current is set based on a % of the rated current which is at rated speed.

Time at peak current is how long the motor can handle the peak current in milliseconds.

The max mechanical speed is typically the bearing limit but you can also set it as maximum speed for the feedback device.

The resistance is in milli-ohms and the inductance in micro-henries.

For saturation/defluxing values, leave this un-checked for permanent magnet (synchronous) motors.

This is an error in the database for US motors and will be corrected in a future revision of the database.

For now, you can just uncheck this.

If this is a standard winding, you do not need to change this unless the motor is force-cooled.

You can change these as needed based on the motor specifications.

 
Step 3 sets allows an optional maximum DC voltage. Thus if the motor is rated for 160vdc like an SM231AE but the drive can

take 230vac, this would prevent a user from enabling the drive with 230vac connected and damaging the motor.

This would cause a 3210 dc link voltage exceeds limit error.

 
Step 4, 5 and 6 are for the motor's current, torque, and speed at 230, 400 and 460volts.

The speed is in rpm, the torque is in milliNewton-meters and the current is in milli-amps.

Again, current is in Arms/phase.

If the motor is not rated for the higher voltage, leave those unchecked.

If this is a standard winding, you do not need to change this, unless the motor is force-cooled.

You can enter these from the Galaxy spreadsheets from your ATC.

 
 
Step 7 is set based on the motor's overtemperature sensor.

If this is based on a standard Parker motor, you don't need to change this.

If the motor doesn't have an overtemperature sensor like the BE16, you can click No.

 
This screen you input the motor's thermal time constant. This is an industry standard specification

for the motor based and is the time it takes to reach 63% of the motor's final temperature given

a constant power input. If you don't have this, you need to contact the motor manufacturer for this.

 
The sensor can be either a PTC or an NTC.

For PTC, you input the resistance at the overtemperature.

If it's only a switch, check the box.

 
Note if you are looking at the motor temperature in the optimization screen under object

684.2 C3.StatusTemperature_Motor this

presumes the motor has a KTY84-130 thermistor.

If it doesn't then the temperature will not be correct.

 
Step 8 is set if the motor has a fail-safe brake or not.

 
If it does, then you can set the set (close) and release (open) time delays.

Note the maximum max current draw is 1.6A.

If the brake current is higher, than you'll need to run the brake output to a relay.

 
Step 9 sets the motor feedback.

The radial button selects the feedback type.

These are straight-forward except SinCos.

This is a Stegmann trademark name for their Hyperface absolute encoders.

This shouldn't be confused with the Heidenhain EnDat which is also a sine-cosine type feedback signal

or a 1volt (peak-peak) sine/cosine encoder.

 
CHM Feedback supported

 
Note the Compax3's have different hardware for the different feedback options.

The F10 is used for resolvers.

The F11 is for the SinCos

The F12 is used for quadrature encoders, EnDat and 1V sine/cosine encoders and analog halls.

 
Below you can see the commutation angle (resolver offset angle), the commutation direction, feedback direction and poles.

On the number of poles, if you don't know, you can set it to 2 and then finish the file.

Download the file to the C3 and then go into the optimization screen to look at the motor's feedback position. Rotate the motor by hand 1 revolution and you can see if it's correct or off by a factor of 2, 3 or more, and then go back and edit the motor file.

These will change based on the feedback type of the motor. For the absolute SinCos and Endat encoders, this will also determine the alignment between the encoder and the motor phases.

 
 
If this custom motor is based on a standard Parker motor, these should be the same as the standard.

To verify, click on Automatic setting of commutation parameters on the bottom.

This will download a configuration to the Compax3 and rotate the motor, determining these directions and angles.

It takes a minute or two to download and will overwrite what's in the drive.

It'll warn you and you can cancel and go back to the main screen to upload.

 
1. Learn commutation values

2. uncheck the discontinuous position. this is only for motor's where it's not possible to measure the position over

an entire revolution

Next it'll start rotating the motor. Click which direction it's rotating.

5. shows whether the commutation or feedback sensor directions had to be inverted. click finish.

 
This takes you back to step 9, populating the feedback direction and commutation angle.

The custom motor file is created when you click Finish.

 
You can then see the motor file under User Defined motors.

The C3 will be blinking Red light (no configuration)

so you'll need to go through the drive configuration to select the new motor file.

 
DRIVE CONFIGURATION & DOWNLOAD

(deactivate limit sensors, HomeMode 35)

click checkbox to open Optimization screen

 
Status Values > Actual postion 680.5

Enable & jog

Note in the base amplifier I10T10 torque mode, you cannot jog from the optimization, you'd have to do atleast velocity mode.

 
Export, Import, Uploading

One last item, if you want to create the motor file and then email it to another user, there's 2 ways to do this.

1. If you have the .c3p file for the drive configuration, when you open this, the C3 ServoManager software looks at the

motor file and if it's not in the motor library, it will add it. So if you already have the file for the Compax3 which is

a .c3p file extension you can email that.

 
2. For only the motor file and not the drive configuration, go back into the MotorManager

(Edit > Start C3MotorManager or via the motor icon on the toolbar)

 
File > Export or right-click on the motor

then exports it as a .xml file

 
The user would then be able to import the motor file with File > Import

 
 
This concludes this module on how to create a custom rotary servo motor file for the Parker Compax3 drive.

 
Have a nice day!