Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Upgrading A/AX Systems
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Upgrading A/AX Systems
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
  • Other-
    • -E Motor Option
    • AC-03 / AC-07 / AC-10 / AC-15 manuals
    • Battery Replacement for 500 or JSI
    • C/CX Suggested Replacements
    • Cage Code
    • Changing the Configuration of the Compumotor Plus
    • Color Code for Stepper Motor External Encoder
    • Compumotor Plus motor internal potentiometers
    • Controller Cable Drawings
    • Custom Products
    • Daedal to Compumotor Cross Reference
    • Daisy chaining AR-C
    • DC Brushed Motor with the Aries & Gemini
    • Drive Input Power
    • Dumping the 3000 memory.
    • EDC TDC XDC VRP PMC
    • Encoder or Resolver?
    • Ferrite absorber
    • Heat Dissipation within Enclosures
    • How do I change the Btorq.dat file?
    • How do I download software from www.parkermotion.com?
    • How do I get support for my Parker SSD / Parvex division products?
    • How Much Power Do I Need?
    • Inertia Ratio
    • Is Parker Compumotor ISO9000 Certified?
    • KH/KS Error 62
    • KH/KS Motors
    • M-Drive/Motor Compatibility and Matching
    • Mating MS Connectors for KH motors
    • Motion Sizer: No motor/gearhead/actuator database error (No TS torque, Divide by 0)
    • My ARC-C or -D does not fit on my motor.
    • Obsolete Products -- 1990 - 1999
    • Obsolete Products -- 2000 and later
    • Offset voltage on the Compumotor Plus
    • Parker MotionSizer: Stationary Rack, Moving Pinion
    • Parker SBC Replacement products
    • PK130M Ordering Part Number Change
    • PK2 Part Number Change(5/9/97)
    • PMC Motion Controllers (PMC20 & PMC10)
    • Printing From Compumotor DOS-based Applications
    • QM Series Motor Information
    • Refurbished Inventory / Educational Discount
    • Setting the deadband on the VAC.
    • Software for the SV
    • Three wire prox sensor color code
    • Torque Margin
    • Transformer Specs
    • Upgrading A/AX Systems
    • VM15 and VM25 Terminal Breakout Modules
    • What is a single and two speed resolver?
    • What is CE, EMC and LVD?
    • What is difference between CD35M and CD60/80M?
    • Windows 2000 locks up when printing
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
Upgrading A/AX Systems

Print Friendly and PDF
If you have an existing A/AX system (which includes an A-Drive or an AX-Indexer/Drive and an A-Motor)...

The A-Drive can be replaced by Zeta Drive. It is a smaller footprint and will fit in the same cabinet space and has the same 25pin D-sub pinout on the front of the drive and also uses the same 120vac plug on the front of the drive making it a very easy upgrade.

The AX-Indexer/Drive can be replaced by an ZETA6000 Indexer/Drive. Note that the ZETA6000 uses a different programming language. However the 6000 series command reference guide gives a cross-over list from the X language commands to the newer and expanded 6000 series language.

However, an A-Motor cannot be replaced by an Zeta-Motor due to the high inductance specs of the A-Motor. An Zeta-Motor would be burned up by the A-Drive.

A-Motors are no longer available for purchase. However, the Zeta-Motors have similar dimensions as the A-series motors. ie A57-51-MO (-MO is motor only) would be replaced by the Zeta57-51-MO.

For full specifications on the A series motors, see the A/AX series user guide. These user guides provide speed-torque curves for the motors and dimension drawings. The Zeta series motors are shown on our website and are the same as the S series or ES series motors.