Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base My 890 control board locked up when updating the firmware, how can I reset the control board?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base My 890 control board locked up when updating the firmware, how can I reset the control board?
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
  • AC and DC Drives and Inverters-
    • AC10+
    • AC30+
    • AC690+ Series+
    • AC890 Series-
      • What are the basic wiring connections for the AC890?
      • What software and communication cable are used for programming an AC890?
      • How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
      • 890 - Interact Xpress with the AC890
      • 890: Why am I getting over-voltage trips?
      • 890PX - Proper ethernet cable - Current Balance, Undervoltage, Missing Phase
      • Can I clone an 890 drive via the Keypad?
      • Can the AC890 be configured as an Active Front End (AFE)?
      • Can the AC890 be used in a load-sharing application?
      • Can the AC890 be used in an electronic lineshaft application?
      • Can the AC890 be used in an encoder following application?
      • Converting .001 file types to .prj file type
      • How can I get the DSE software?
      • How can I get the DSELite software?
      • How can I load different firmwares?
      • How can I recover from a COMMS CODE N error on the AC890
      • How can I troubleshoot Firewire problems?
      • How can the 890 family be configured?
      • How can the AC890 be reset to factory defaults?
      • How can you add an item to the OPERATOR MENU in an AC890?
      • How do I determine an 890 drive TAG NUMBER so it can be used in DSE890?
      • How do I know what firmware revision my AC890 is?
      • How do I make an 890 Phase move?
      • How do I startup & troubleshoot a PMAC motor on the 890?
      • Is the keypad detachable during operation?
      • Is there any additional information on troubleshooting 690+ and AC890 Frame K drives? (copy)
      • My 890 control board locked up when updating the firmware, how can I reset the control board?
      • The AC890 is enabled, and START is true, but the motor runs slow with high torque. Why?
      • The AC890's DC bus voltage is extremely high on power-up. Why?
      • The AC890PX DC bus voltage is extremely high on power up. Why?
      • What are the minimum and maximum 3-phase input voltage ratings on an 890SD, CD, CS and PX?
      • What are the reference power supplies available to terminal connections on the AC890?
      • What can I use to replace an 8902/RR/00/00?
      • What configurable I/O is available on the AC890?
      • What is the current overload rating for the AC890 drive?
      • What is the maximum operating altitude for the AC890?
      • What is the operating temperature for the AC890?
      • What kind of I/O is available on the AC890?
      • What options can be added to the AC890/890PX?
      • What safety standards does the 890 meet?
      • What slots I can put options in, and how do I install them?
      • What types of speed feedback are supported for the AC890?
      • Where do I find default configurations?
      • Why am I getting an Incompatible Power Board message?
      • Why can't I connect to my AC890 drive with the USB cable
      • Why is my AC motor running hot?
      • Why is the LED on the control board flashing 50% red and 50% green?
      • Why won't DIN3 stop my 890 drive with a default configuration in remote mode?
      • Why won't my AC890 inverter run my motor?
      • AH469479U001 card - Use 8903/??/00/00 when ordering replacements
      • AH469910U001 - Use 8904/A/US/03/00 or 8904/A/US/03/83 to order replacements
      • How do I convert AC890 Europe part numbers to US part numbers?
      • HOW DOES THE INVERSE TIME (OVERLOAD) FUNCTIONALITY PROTECT THE DRIVE (890)?
      • Runtime alert when connecting to or downloading a project to an 890 drive - DSEv3.10
    • DC590+ Series+
    • TS8000, DSI3, & DSI8000+
    • Legacy/Discontinued VFD Products+
    • What software and communication cable are used for programming?
    • DSE Lite and Drive Firmware Compatibility
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+, 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
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
My 890 control board locked up when updating the firmware, how can I reset the control board?

Print Friendly and PDF

When upgrading the firmware on an 890 Control board, in rare cases, this process may fail, thus leaving the control board in a state where DSE can't communicate to this board. This procedure will explain how to reset the board, so DSE can try to communicate to it.

Procedure:

  1. Remove the 890 control board from the drive. Determine if the control board is a rev 2 (see photo on page 2) or a rev 3 control board. See the attached pictures. Make sure to remove power to the drive before removing the control board. Locate the PLG silkscreen on the board. View the pictures and look for the RED Arrow. It is located behind the X15 terminal block on the rev 3 control board. This may require the removal of the Firewire option card 8903/FA.
Figure 1: For a Rev 3 control board AH469910.
  • Follow these step-by-step instructions exactly.
  • Strip the ends of a 12” piece of wire, fold it in half and insert the ends into both holes, of the 2 connections pads PLG. View the pictures and look for the RED Arrow. The arrow points to pads PLG1 on the Rev 3 board and PLG6 on the rev 2 board.
  • Once the wires are inserted to PLG, insert the control board back into the drive chassis. Route the wires to the outside of the drive control board.
  • Make sure DSE is closed. Connect the USB cable to the USB port on the 890 drive.
  • Launch DSE and go to COMMAND / INSTALL FIRMWARE.
  • Select the firmware to be installed. Do NOT press the INSTALL button yet. (It may take up to 1 minute for the window to appear).
  • Apply power to the 890 drive control board.
  • Carefully pull the wire out of the drive, thus removing the wire from the connections pads PLG.
  • In DES press the INSTALL buttion.
  • Once the firmware is installed, install the configuration into the control board.
  • Reinstall the Firewire option card 8903/FA if it was removed. Make sure to remove power to the drive before removing the control board.
Figure 2: For a Rev 2 control board AH465820 insert jumper wire into PLG6.
  • [QuickLink for the 890 on Parker.com] - Manual, QuickStarts, Product Support, etc
  • [QuickLink for the 890PX on Parker.com] - Manual, QuickStarts, Product Support, etc

8NOV2016 LS

  • board
  • fail
  • reset
  • firmware
  • control
  • locked
  • 890