Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base The AC890PX DC bus voltage is extremely high on power up. Why?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base The AC890PX DC bus voltage is extremely high on power up. Why?
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
  • AC/DC Industrial Drives-
    • AC10+
    • AC30+
    • DC590+ Series+
    • AC890 Series-
      • AH469479U001 card - Use 8903/??/00/00 when ordering replacements
      • AH469910U001 - Use 8904/A/US/03/00 or 8904/A/US/03/83 to order replacements
      • What are the basic wiring connections for the AC890?
      • What software and communication cable are used for programming an AC890?
      • How to Install and Extract Parameters From a 890 or 890PX Drive Using DSE Lite?
      • 890 - Interact Xpress with the AC890
      • 890: Why am I getting over-voltage trips?
      • 890PX - Proper ethernet cable - Current Balance, Undervoltage, Missing Phase
      • Can I clone an 890 drive via the Keypad?
      • Can the AC890 be configured as an Active Front End (AFE)?
      • Can the AC890 be used in a load-sharing application?
      • Can the AC890 be used in an electronic lineshaft application?
      • Can the AC890 be used in an encoder following application?
      • Converting .001 file types to .prj file type
      • How can I get the DSE software?
      • How can I get the DSELite software?
      • How can I load different firmwares?
      • How can I recover from a COMMS CODE N error on the AC890
      • How can I troubleshoot Firewire problems?
      • How can the 890 family be configured?
      • How can the AC890 be reset to factory defaults?
      • How can you add an item to the OPERATOR MENU in an AC890?
      • How do I determine an 890 drive TAG NUMBER so it can be used in DSE890?
      • How do I know what firmware revision my AC890 is?
      • How do I make an 890 Phase move?
      • How do I startup & troubleshoot a PMAC motor on the 890?
      • Is the keypad detachable during operation?
      • Is there any additional information on troubleshooting 690+ and AC890 Frame K drives? (copy)
      • LA471585 I/O Break-Out Module (Discontinued)
      • My 890 control board locked up when updating the firmware, how can I reset the control board?
      • The AC890 is enabled, and START is true, but the motor runs slow with high torque. Why?
      • The AC890's DC bus voltage is extremely high on power-up. Why?
      • The AC890PX DC bus voltage is extremely high on power up. Why?
      • What are the minimum and maximum 3-phase input voltage ratings on an 890SD, CD, CS and PX?
      • What are the reference power supplies available to terminal connections on the AC890?
      • What can I use to replace an 8902/RR/00/00?
      • What configurable I/O is available on the AC890?
      • What is the current overload rating for the AC890 drive?
      • What is the maximum operating altitude for the AC890?
      • What is the operating temperature for the AC890?
      • What kind of I/O is available on the AC890?
      • What options can be added to the AC890/890PX?
      • What safety standards does the 890 meet?
      • What slots I can put options in, and how do I install them?
      • What types of speed feedback are supported for the AC890?
      • Where do I find default configurations?
      • Why am I getting an Incompatible Power Board message?
      • Why can't I connect to my AC890 drive with the USB cable
      • Why is my AC motor running hot?
      • Why is the LED on the control board flashing 50% red and 50% green?
      • Why won't DIN3 stop my 890 drive with a default configuration in remote mode?
      • Why won't my AC890 inverter run my motor?
      • How do I convert AC890 Europe part numbers to US part numbers?
      • HOW DOES THE INVERSE TIME (OVERLOAD) FUNCTIONALITY PROTECT THE DRIVE (890)?
      • Runtime alert when connecting to or downloading a project to an 890 drive - DSEv3.10
    • AC15/AC20+
    • Legacy/Discontinued Products+
    • What software and communication cable are used for programming?
    • DSE Lite, Drive Firmware, and Project Compatibilities
    • How do I update my DSE, DSELite, DSI3, DSI8000, or DSD software?
    • How do I migrate my DSE (DSE890), DSELite, DSD software to a new computer?
    • Why does DSE or DSELite crash when creating or opening a new project?
    • How can I flash the LinkNet Techbox firmware?
    • What is an Autotune and how do I run one?
    • Do you have CAD available for SSD Products? AC10, AC30, 590+, 650 (OBX), 690+ (OBX), 890
    • 6053...6054...6055...? Techbox options
    • How do I cross a Legacy or Parker European part number to modern Parker North American part numbers?
    • Maximum Speeds for VFD drives
    • Replacement keypad part numbers (590+ / 690+ / 890 / AC30 / AC10)
    • What is 'BOOST' in Parker VFD drives?
    • 6053 DNET Techbox Firmware Incompatibilities
    • DESAT (OVER I) Fault
    • Constant Torque (CT) versus Variable Torque (VT) in VFDs
    • DSE890 and DSELite Ethernet Connection Port Numbers
    • ACxx scope tool problems with Windows 11
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
The AC890PX DC bus voltage is extremely high on power up. Why?

Print Friendly and PDF

SEE THE ADJACENT FAQ IF YOU HAVE A STANDARD 890 INSTEAD.

  1. This can mean the Y-caps are creating a voltage multiplier.
    1. This can be a result of the AC890 being used as an AFE (Active Front End).
      (Typically when drives are going to be used in an AFE Application they are ordered with the 007 option)
    2. This can occur if the drive is connected to a transformer with "Open-Delta" or "Corner-Grounded Delta" windings.
  2. The Y-Caps can be disconnected.

Warning:
Removal of the 'Y' capacitors invalidates conformance to the EMC standards stated on the Declaration of Conformity in the product manual. The CE mark remains on the product as this is for product electrical safety.
B-D frames = software
E-K frames = same as 690+

BROKEN IMAGE -- DCLIFFE

Procedure:

  1. Remove power to the 890PX.
  2. Locate the 3 CD Modules (Output Modules) as each one will have to be removed, to be modified.
  3. Remove one of the three CD Modules. To remove the CD Module unplug the cables from the front of the module. Unscrew the left screw 5 turns then unscrew the right screw 5 turns. Repeat this procedure until the module is removed. The module screws need to be removed evenly, thus do not exceed 5 turns per screw at a time. Once removed rotate the module, to view the back of it as shown below.

BROKEN IMAGE -- DCLIFFE

  • Locate the EMC Capacitor jumper as shown below. It is in the top middle of the CD Module.

BROKEN IMAGE -- DCLIFFE

  • With a set of needle nose pliers, grab a hold of the metal jumper, and completely remove this metal jumper.

BROKEN IMAGE -- DCLIFFE

  • Reinstall the module into the 890PX. Keep in mind the 5 turns per screw, at a time procedure. See step 3.
  • Repeat this procedure for the remaining 2 CD Modules.

  • [QuickLink for the 890PX on Parker.com] - Manual, QuickStarts, Product Support, etc

9NOV2016 LS

  • voltage
  • DC bus
  • 890PX
  • high
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply