Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base User Function Block: Read Actual Torque
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base User Function Block: Read Actual Torque
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)-
        • Acrobasic commands for IEC PLC
        • ACRView 6.4.1 Runtime Error for 9600 and 9640
        • ACRView IEC Editor not Compatible with Win10
        • Converting ACR9600 Projects to ACR9000 Projects
        • General Function Block Behavior
        • How to add multiple outputs in ACR IEC PLC ladder programs
        • How to change the Task Type or Task Speed
        • How to change velocity on the fly
        • How to home to a limit in ACR96xx
        • How to Modify a ACR-View project (9600) AcroBasic only programs for Win10
        • How to run an AcroBasic program from IEC PLC
        • How to start the IEC PLC on controller power-up
        • How to use Direct Variable references in ACR IEC PLC
        • IEC Error Message: No valid license for the current hardware
        • Invert Motion Direction in IEC PLC
        • Is there a First Scan flag in the IEC PLC
        • PLCOpen State Machine
        • Set Compax3-EPL Current Limit
        • User Function Block : Excess Position Error Response
        • User Function Block : Moving Average
        • User Function Block : Rotary Axis Position
        • User Function Block: Read Actual Torque
        • User Function Block: Software Limits
        • Using arrays in IEC PLC
        • Using the IEC Debug Window and Watch Lists
        • Variable Declarations in IEC Languages
        • VIDEO: How to import function blocks into ACR IEC_PLC projects
        • What is a Moving Segment Error?
        • Why is the IEC PLC making the axis to move farther and faster than programmed?
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
User Function Block: Read Actual Torque

Print Friendly and PDF

Products: ACR9600, ACR9630, ACR9640

AXIS_READTORQUE is a user function block that enables the user to monitor actual torque output of an axis. Download the code here : Axis_ReadTorque

The block reports the Final Ouput Signal parameter. Read here for full explanation. User can also input a ScaleFactor that is multiplied by the final output signal allowing the user to represent Torque or Force in units that are meaningful to the application.

 

VAR_IN_OUT
AXIS AXIS_REF Axis Reference
VAR_INPUT
ENABLE BOOL Enables the block to perform the read
ScaleFactor REAL Default = 1.0. This value is multipled by FINALOUTPUT to produce ActualTorque
VAR_OUTPUT
VALID BOOL Block is reading properly
FINALOUTPUT REAL Read here
ActualTorque REAL FinalOutput Signal x ScaleFactor
Error BOOL Signals that error has occurred within function block
ErrorID WORD Error identification

 

 

jw Mar-2013

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply