Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base User Function Block : Moving Average
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base User Function Block : Moving Average
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)-
        • Acrobasic commands for IEC PLC
        • ACRView 6.4.1 Runtime Error for 9600 and 9640
        • ACRView IEC Editor not Compatible with Win10
        • Converting ACR9600 Projects to ACR9000 Projects
        • General Function Block Behavior
        • How to add multiple outputs in ACR IEC PLC ladder programs
        • How to change the Task Type or Task Speed
        • How to change velocity on the fly
        • How to home to a limit in ACR96xx
        • How to Modify a ACR-View project (9600) AcroBasic only programs for Win10
        • How to run an AcroBasic program from IEC PLC
        • How to start the IEC PLC on controller power-up
        • How to use Direct Variable references in ACR IEC PLC
        • IEC Error Message: No valid license for the current hardware
        • Invert Motion Direction in IEC PLC
        • Is there a First Scan flag in the IEC PLC
        • PLCOpen State Machine
        • Set Compax3-EPL Current Limit
        • User Function Block : Excess Position Error Response
        • User Function Block : Moving Average
        • User Function Block : Rotary Axis Position
        • User Function Block: Read Actual Torque
        • User Function Block: Software Limits
        • Using arrays in IEC PLC
        • Using the IEC Debug Window and Watch Lists
        • Variable Declarations in IEC Languages
        • VIDEO: How to import function blocks into ACR IEC_PLC projects
        • What is a Moving Segment Error?
        • Why is the IEC PLC making the axis to move farther and faster than programmed?
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
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
  • AC/DC Industrial Drives+
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
User Function Block : Moving Average

Print Friendly and PDF

Products: ACR9600, ACR9630, ACR9640

Moving_Average is a user function block that calculates a rolling average of REAL values. With input N, user can select the number of samples to be averaged with a maximum of 128.

Download the code here : Moving_Average

 

-->
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply