Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base User Function Block : Excess Position Error Response
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base User Function Block : Excess Position Error Response
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)-
        • Acrobasic commands for IEC PLC
        • ACRView 6.4.1 Runtime Error for 9600 and 9640
        • ACRView IEC Editor not Compatible with Win10
        • Converting ACR9600 Projects to ACR9000 Projects
        • General Function Block Behavior
        • How to add multiple outputs in ACR IEC PLC ladder programs
        • How to change the Task Type or Task Speed
        • How to change velocity on the fly
        • How to home to a limit in ACR96xx
        • How to Modify a ACR-View project (9600) AcroBasic only programs for Win10
        • How to run an AcroBasic program from IEC PLC
        • How to start the IEC PLC on controller power-up
        • How to use Direct Variable references in ACR IEC PLC
        • IEC Error Message: No valid license for the current hardware
        • Invert Motion Direction in IEC PLC
        • Is there a First Scan flag in the IEC PLC
        • PLCOpen State Machine
        • Set Compax3-EPL Current Limit
        • User Function Block : Excess Position Error Response
        • User Function Block : Moving Average
        • User Function Block : Rotary Axis Position
        • User Function Block: Read Actual Torque
        • User Function Block: Software Limits
        • Using arrays in IEC PLC
        • Using the IEC Debug Window and Watch Lists
        • Variable Declarations in IEC Languages
        • VIDEO: How to import function blocks into ACR IEC_PLC projects
        • What is a Moving Segment Error?
        • Why is the IEC PLC making the axis to move farther and faster than programmed?
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
User Function Block : Excess Position Error Response

Print Friendly and PDF

Products: ACR9600, ACR9630, ACR9640

AXIS_EXC_Response is a user function block that adjusts the settings for Excess position error checking. With EnableEXC=True, drive will be disabled if allowable error is exceed. Download the code here : Axis_EXC_Response

See also Acrobasic command EXC

VAR_IN_OUT
Axis AXIS_REF Axis Reference
VAR_INPUT
Execute BOOL Assigns settings at the rising edge
EnableEXC BOOL Enables Excess Position Error Response
MaxPositiveError REAL allowable error in postive direction, user units
MaxNegativeError REAL allowable error in Negative direction, user units
VAR_OUTPUT
Done BOOL Limits have new assignment

 

jw -Apr-2013

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply