Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Meaning of the Status LEDs
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Meaning of the Status LEDs
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)-
      • Controller (CE)+
      • Drive only (AE,AR, SE, SR)-
        • 3rd party resolver with resolver based Aries drive
        • Aries ARxxSE/ARxxSR tuning for Step/Direction
        • Aries Drive Family Letter of Volatility
        • Aries encoder output - Quadrature or SSI?
        • Galil DMC to Aries Connections
        • Hall-only Commutation
        • Meaning of the Status LEDs
        • Operating System Update Notes
        • RS485: PC connections through B&B Electronics 485BAT3 to Aries
        • Using single-ended inputs with the Aries
        • VIDEO: How to Configure Aries Servo Drives
        • What does it mean when my left LED is flashing 1 yellow and 5 green?
        • Why are Aries motor parameters missing?
        • Why is my Aries torque-drive clicking?
        • Why is my enable LED flashing?
        • Why is there a delay before motion on my Aries?
      • EPL+
      • AR-20 and AR-30 minimum AC voltage
      • Absolute Encoders & Drive Compatibility
      • Aries - MaxPlus (MPM) Encoder Option 1 Connection
      • Aries - MaxPlus (MPM) Resolver Option 1 Connection
      • Aries Brake Delay
      • Aries Drive: Connector Part Numbers
      • Bayside GM Gearmotor Files for Aries
      • Cables to connect GM motors to Parker Drives
      • Can I use Aries drives with MX80L linear motor stages?
      • DTALK with Aries 3.32 & higher firmware
      • E27 Bridge Hardware Fault
      • E54 Feedback Loss Fault - 5 Green Flash 1 Yellow
      • How do I power an ARIES with 3 phase?
      • How do I know Aries SFB is set to auto-detect?
      • How to Update Operating System (Firmware)
      • Manual Alignment Procedure
      • Peak Current Time from Compumotor Drives
      • Aries drive won't enable
      • Selecting a Fuse
      • Using R100,R150 and R200 with Aries
      • Aries (AR-xxAE or AR-xxSE) Recommended Replacements
      • Aries 2000/3000 watt Replacements (AR-20AE, AR-30AE, AR-20SE, AR-30SE)
      • Aries Resolver Replacement (AR-01AR, AR-02AR, AR-04AR, AR-08AR, AR-13AR, AR-01SR, AR-02SR, AR-04SR, AR-08SR, AR-13SR)
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Meaning of the Status LEDs

Print Friendly and PDF

The Aries drive has two bi-color LEDs. The LED on the left displays yellow or green colors; The LED on the right displays red or green colors. The following tables describe LED illumination states and the conditions they indicate:

 

Power On Sequence:

1. The right led will be Red (left off)

2. Left LED will be Yellow during the boot load (right off).

3. Then it'll go to the Normal operation LEDs.

 

If the Aries has not been configured for the motor: the Aries drive will be in Other Fault - Yellow & 4 Green (flashing), Red.

PLEASE NOTE: Some versions of the Aries Drive Quick Reference Guide may incorrectly state that that the left LED status of Yellow and 4 Green (flashing) as a Low Voltage Fault..

If your drive status does indicate Other Fault: then connect a communication cable to the drive and query the drive for the actual error with the ERROR command or look in the status panel of the Aries Support Tool  software.

 

This related FAQ shows how to connect to an Aries drive and the Aries Support Tool (AST) software:

VIDEO: How to Configure Aries Servo Drives

 

Less common status but also valid:

LED-Left LED-Right Drive Status-What it means
Off Green (flash) Foldback Mode (activated with DIFOLD1)
Green&Red (flash) Off Auto-commutate (rev 3.11 or higher)

These are not noted yet in the user manual but in the firmware release notes, available in the download of the firmware.

9/3/14jh updated

1/10/18jh updated adding less common

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply