Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base InteractX Training - Tag Rules (Tag Sharing) Examples
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base InteractX Training - Tag Rules (Tag Sharing) Examples
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX-
      • InteractX Misc - Cannot find product code for Win9X/NT
      • InteractX Misc - Comm Server Connection to Allen Bradley Logix Processors
      • InteractX Misc - Comparison of valid operators in InteractX versus Interact
      • InteractX Misc - How do I get my InteractX project off of my old unit and onto my new IPX Powerstation?
      • InteractX Misc - How to order InteractX Upgrades
      • InteractX Misc - How to re-register older versions of Interact X (versions 1.x through 3.4)
      • InteractX Misc - How to Start InteractX Runtime Project Automatically?
      • InteractX Misc - Is InteractX Version 1.x, 2.x or 3.x Compatible with Windows 7 or Later?
      • InteractX Misc - InteractX Browser Tool used to display Xpress or PFD screens impacted by Adobe Flash EOL.
      • InteractX Misc - InteractX Software Archive
      • InteractX Misc - Language Multi-Byte Character Support for ASCII Input - Cyrillic, Asian etc...
      • InteractX Misc - Migrating InteractX from legacy HMI and PC systems to Current Hardware and Windows OS Versions
      • InteractX Misc - Uploading and downloading InteractX projects over Ethernet
      • InteractX Misc - Uploading and downloading InteractX projects with a USB drive
      • InteractX Misc - User Configurable Driver User Guide (UCON)
      • InteractX Misc - Version 4.0/4.1 Security Device Questions
      • InteractX Misc - Where does my Powerstation store my InteractX license activation?
      • InteractX Misc - Which HMI runs InteractX?
      • InteractX Software - Complete Modbus/RTU Addressing Example for P Series Indexer Drive
      • InteractX Software - Express Browser Demo
      • InteractX Software - How do I control the Lens States for an Indicator tool in Int X?
      • InteractX Software - How to Shutdown InteractX and Windows
      • InteractX Software - How to Use Existing Recipes as Items within a New or Modified Recipe
      • InteractX Training - Creating and Configuring Event Logs in InteractX
      • InteractX Training - Creating Databases and Tables in InteractX
      • InteractX Training - Database Basics
      • InteractX Training - Getting Started with Quicklogging
      • InteractX Training - Print a Report from InteractX using a VBA form to create your Report layout and VBA logic to populate it.
      • InteractX Training - Recipe Training Module
      • InteractX Training - SQL Database - Basics to use Logging Tools and how to use VBA SQL Script to read data back.
      • InteractX Training - Tag Rules (Tag Sharing) Examples
      • InteractX Training - VBA Login Example
      • InteractX Troubelshooting - ACR9000 CIP Communications stop on all devices when one CIP device goes offline
      • InteractX Troubleshooting - Version 4.1 will not automatically start on my Windows 10 Runtime PC due to requiring elevated privileges
      • InteractX Troubleshooting - Alarm History Viewer not working as expected (InteractX version 4.1)
      • InteractX Troubleshooting - Allen Bradley ControlLogix Driver Compatibility Issues.
      • InteractX Troubleshooting - Can not get License Activation to work on HMI/PC running InteractX version 1.x to 3.4
      • InteractX Troubleshooting - Com Server Error Log
      • InteractX Troubleshooting - COMM Server still using old configuration after download of application with changes to communication settings.
      • InteractX Troubleshooting - ControlLogix Driver unable to upload tags from Device (PLC) unable to read known good tags from processor.
      • InteractX Troubleshooting - CTC Runtime Data Error Symbols (! ? broken pencil etc)
      • InteractX Troubleshooting - Error Initializing VBA when going into run mode or opening the VBA Editor in Development
      • InteractX Troubleshooting - Hardware License Not Found - One Hour Runtime - Remote Desktop
      • InteractX Troubleshooting - InteractX 4.0 HASP key driver Aladdin vs Sentinel (NOTE: IntX4.1 for Windows 10 uses Sentinel Drivers)
      • InteractX Troubleshooting - Invalid Page Fault in the NTOSKERNEL.EXE (old PC/PX models)
      • InteractX Troubleshooting - Loss of Characters on the Pop-up Keyboard, Keypad, etc.
      • InteractX Troubleshooting - Problems with large number accuracy
      • InteractX Troubleshooting - Downloaded InteractX application with Ethernet driver fails to connect even though ping is successful and works otherwise
      • InteractX Troubleshooting - VBA is not working on my new Windows 7/8.1/10 PC (Versions 4.0 / 4.1)
      • InteractX Troubleshooting - Unable to get Data Connection to Xpress tags to work.
      • InteractX Troubleshooting - Why can't I log data with Microsoft Jet (MDB file) in InteractX?
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)+
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
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
InteractX Training - Tag Rules (Tag Sharing) Examples

Print Friendly and PDF

The attached file is a sample InteractX project.  Download and save it in your computer and then do a 'Restore Project' on this archived folder to open it in the InteractX development software.

The Tag Rules are included on one of the project panels for reference.  See the Tag Editor for how the tag rules were applied and the math functions being done.

Tag_Rules_Examples

Logic Example - The tag Set_All is assigned to the button labeled Set_All.  The tag is then also used in the addresses for tags Bit128, Bit132, and Bit140, which are tied directly to their respective hardware memory locations in the ACR controller with the following syntax:

'ACR.ACR1.BIT128' = Set_All

'ACR.ACR1.BIT132' = Set_All

'ACR.ACR1.BIT140' = Set_All

The Set_All button is a latch type of button.  The Clr_All button unlatches the Set_All button which in turn sets all three user bits back to zero.

The OR, AND, XOR indicators simply apply advanced logic math equations to the Bit128, Bit132, and Bit140 values.  See the Tag Editor for these equations.

Values Example - This panel is simple example of using a single numeric entry tool to set a numeric value to two parameters in the controller. 

The numeric entry tool is tied to the tag Set_Vel.  Then the controller parameters are set in tags AX0_Vel and AX1_Vel with the following addresses:

'ACR.ACR1.P12346' = Set_Vel

'ACR.ACR1.P12602' = Set_Vel

Math Example - This panel does some creative things using the tag rules and the simulator driver to simulate data that would normally be changing in the controller.  The ACR system timer is used and a couple of user parameters are used. 

Normally these functions would be done in the controller but were added to this sample simply as an illustration and so that no programs would need to be running in the controller to make this sample 'work'.

Key Words - tag rules tag sharing

glh May 2013