Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base VIDEO: How to set your PC's Ethernet IP address
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base VIDEO: How to set your PC's Ethernet IP address
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
  • General Technology Information-
    • How do I determine the MAC address for my unit?
    • Install the network card in Windows NT.
    • Servers Services error on boot up in NT
    • Comparison of Motor Technologies: Servo, Stepper, Stepper with Encoder
    • How to check if a USB to serial converter has an FTDI chipset
    • Modbus Basics
    • Recommended Installation Practices for Robust Systems
    • Video: Different Servo Loop Control Schemes, Drives with Fieldbus vs Motionbus
    • Video: Electric Motors Overview: Brushed, Stepper and Brushless
    • Video: Gearhead Engineering Reference
    • Video: How a Brushed Motor works
    • Video: How a Drive controls current in a stepper or servo motor
    • Video: How a Servo Motor works
    • Video: How a Step Motor works
    • Video: How is a Brushed Motor Constructed?
    • Video: How is a Servo Motor Constructed?
    • Video: How is a Step Motor Constructed?
    • Video: How Servo Loops and PID works (Torque, Velocity, Position)
    • VIDEO: How to set your PC's Ethernet IP address
    • VIDEO: How to troubleshoot RS232 serial communications
    • Video: IO Wiring: What is NPN PNP Sinking Sourcing?
    • Video: Servo Motor Feedback (Encoders, Halls & Resolvers) & Commutation
    • Video: Step Motor Resonance
    • Video: Step Motor Windings explained: Series vs Parallel
    • What is EtherCAT? How does it work? How does it help me?
    • What is IEC61131-3? What is PLCopen?
    • Windows 10 support (Win10)
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
VIDEO: How to set your PC's Ethernet IP address

Print Friendly and PDF

How to set your PC's Ethernet (TCP/IP) address in order to communicate to ACR7000, ACR9000, ACR9600, IPA, PSD, Aries Controller, PAC, Compax3 I30, 6K, Gemini6K, Interact Xpress or InteractX


 MOBILE USERS CLICK HERE

Procedure for Windows7:
Connect ethernet cable to PC and controller/drive

1. Open the Control Panel on your PC by clicking Start / Windows button and click Control Panel.


2. Click Network and Internet.
3. Click Network and Sharing Center.
4. Click Local Area Connection.
5. Click Properties.
6. Select Internet Protocol Version 4 (TCP/IPv4) and click Properties.

7. Click the radio button next to Use the following IP address and type in an IP address with the same first three octects as the default IP address. Set the last octect to a number different from the number set on the controller/drive. Making the last octect different gives the product and PC different IP addresses in the ethernet network. Valid range is 1 to 254. Using 000 or 255 is not valid. As an example, the PC's IP address is set to 192.168.100.25


8. Set the Subnet mask value to 255.255.255.0
The PAC320 should be set to 255.255.0.0

9. Click OK. These windows can now be closed. You now can ping the controller/drive and should be able to use the controller/drive software to connect.

4/12/14jh
updated 12/14jh - win7 procedure