Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base VIX Servo: How to Home to a Hard Stop
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base VIX Servo: How to Home to a Hard Stop
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)+
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)-
      • Analog control of a Vix stepper
      • Can an Intelligent ViX-In be Programmed as a Drive
      • Configuring the ViX-drive
      • DC Brushed Motor with a ViX
      • Does the Vix have software limits?
      • Downloading Programs
      • Easi-V with Windows 7 or Windows 10
      • Homing move not complete
      • How Do I Check encoder position?
      • How to program an intelligent ViX Stepper as a Step & Direction
      • LOADENC and SCALE Commands
      • Running a Rotary Motor with a ViX-xH
      • Sample Program - Move Continuously, Stop on Inputs
      • VIX - RS232 connections
      • VIX Servo: How to Home to a Hard Stop
      • VIX Update Rates
      • ViX User Variables
      • ViX CANopen / RS-485 option
      • ViX Easi-V Error Message: Invalid data read for limits mode
      • ViX Encoder Resolution / Input Frequency
      • ViX Motor files for non-preferred BE windings
      • ViX Tuning
      • ViX servo drive Z channel encoder output
      • ViX-RJ45 RS-232 Daisy-Chain Cables
      • ViX: Connector Part Numbers
      • ViX: ViX Update Rates
      • Vix- Option 1 (MPM) Encoder Hardware Setup
      • Vix-IE with Brushed motor and Encoder
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
VIX Servo: How to Home to a Hard Stop

Print Friendly and PDF

Below is some sample code on how to home to a hard stop using the ViX servo controller.

NOTE:  Use a low speed and set a low torque limit and GP gain for testing. Your customer will need to calculate the correct CR value. Limiting your total torque to 10 % should be a good starting point to prevent damage. The scale of the CR value is +/-931903, reference this value to the peak current setting of the VIX.

Sample code: 

;Torque/Current limit example
;This program example shows a drive running up to a torque
;limit.

 

1K  ;Kill all programs.
1CLEAR(ALL) ;Clear all programs.
1START:  ;Start program is required to declare run label.
1DECLARE(RUN) ;Declare "RUN" label.
1END


1RUN:  ;"RUN" program.
1MC  ;Set continous motion.
1V1  ;Set velocity to 1 rps.
1D-123  ;Force distance to negative direction.
1W(CQ,0) ;Write the value of continous execution to 0.
1ON  ;Turn on drive.
1G  ;Run axis.
1R(CR)  ;Print current reference.
1TR(CR,<,-10000);Trigger when system current reference is less
  ;then -10000.
1R(CR)  ;Print current reference.
1OFF  ;Turn off axis.
1END

29-Jul 2016 nc

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply