Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Aries-EPL Digital Filtering
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Aries-EPL Digital Filtering
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
  • Servo Drives and Servo Drive/Controllers-
    • Aries Drive (Discontinued)-
      • Controller (CE)+
      • Drive only (AE,AR, SE, SR)+
      • EPL-
        • Aries Ethernet Powerlink (EPL) Replacement (AR-04PE, AR-08PE, AR-13PE)
        • Aries-EPL Digital Filtering
        • How to Convert an AriesCE to AriesPE (AriesEPL)
      • AR-20 and AR-30 minimum AC voltage
      • Absolute Encoders & Drive Compatibility
      • Aries - MaxPlus (MPM) Encoder Option 1 Connection
      • Aries - MaxPlus (MPM) Resolver Option 1 Connection
      • Aries Brake Delay
      • Aries Drive: Connector Part Numbers
      • Bayside GM Gearmotor Files for Aries
      • Cables to connect GM motors to Parker Drives
      • Can I use Aries drives with MX80L linear motor stages?
      • DTALK with Aries 3.32 & higher firmware
      • E27 Bridge Hardware Fault
      • E54 Feedback Loss Fault - 5 Green Flash 1 Yellow
      • How do I power an ARIES with 3 phase?
      • How do I know Aries SFB is set to auto-detect?
      • How to Update Operating System (Firmware)
      • Manual Alignment Procedure
      • Peak Current Time from Compumotor Drives
      • Aries drive won't enable
      • Selecting a Fuse
      • Using R100,R150 and R200 with Aries
      • Aries (AR-xxAE or AR-xxSE) Recommended Replacements
      • Aries 2000/3000 watt Replacements (AR-20AE, AR-30AE, AR-20SE, AR-30SE)
      • Aries Resolver Replacement (AR-01AR, AR-02AR, AR-04AR, AR-08AR, AR-13AR, AR-01SR, AR-02SR, AR-04SR, AR-08SR, AR-13SR)
    • Compax3+
    • Dynaserv (Discontinued)+
    • Gemini (Legacy)+
    • IPA Drive/Controller+
    • P Series+
    • PSD - High Performance Servo Drive+
    • ViX (Legacy)+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Aries-EPL Digital Filtering

Print Friendly and PDF

The Aries-EPL drives do have digital filtering available for the control loop.  These are not shown in the existing Aries-EPL documentation at this time but are included in the current Operating Systems. 

The setup needs to be done talking to the specific EPL drive through the ACR's Talk To feature via the EPL network (see the ACR-View Terminal window for the Talk To feature).

Here are the applicable commands (can also be accessed via the parameter numbers):

DNOTAD Notch Filter A Depth  (parameter C30)

DNOTAF Notch Filter A Frequency (parameter C31)

DNOTAQ Notch Filter A Quality Factor (parameter C32)

  

DNOTBD Notch Filter B Depth (parameter C33)

DNOTBF Notch Filter B Frequency (parameter C34)

DNOTBQ Notch Filter B Quality Factor (parameter C35)

 

DNOTLD Notch Lead Filter Break Frequency (parameter C36)

 

DNOTLG Notch Lag Filter Break Frequency (parameter C37)

 

You can reference the non-EPL Aries user guide to see these specific commands for further details on how they work.   Aries AE/SE User Guide

Note - Aries-CE units implement the ACROBASIC filtering commands rather than the commands shown here.  Refer to the ACR-View help files for those commands.

 

glh 10/2014  Oct 2014

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply