Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base Is there a Windows7 / Windows 10 driver for my PHM / PM1 touchscreen interface?
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base Is there a Windows7 / Windows 10 driver for my PHM / PM1 touchscreen interface?
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
  • Visualization and Human Machine Interface (HMI)-
    • General Communications Driver+
    • Interact (Legacy)+
    • InteractX+
    • Interact Xpress+
    • IX / PCA+
    • IPX / IPC (Discontinued)+
    • PHM / PM1 Industrial Monitors (Discontinued)-
      • Is there a Windows7 / Windows 10 driver for my PHM / PM1 touchscreen interface?
      • Using a PHM monitor with a headless XPR/XPR2 unit
      • What can replace a PM1 or PHM industrial touchscreen monitor?
    • PA / PS / P1-P9 (DOS-based Interact HMI)+
    • PX / HPX InteractX HMIs (Discontinued)+
    • CE Declaration of Conformity for HMI
    • CTC/HMI: Connector Part Numbers
    • My HMI will not boot. Says no boot device found even after I ran the Flashback utility for my model HMI
    • Parker Factory Display Troubleshooting - Step 3 Error when clicking Design in your PFD Project
    • Latest versions of HMI software packages
    • Failed install / Can't install because of pending/suspended action. Can't uninstall and Installshield quits or throws an error and can not continue.
    • PowerStation Accessories - Mounting kits, Connectors, Protective Overlays
    • What HMI software runs on which models of HMI? (Consolidated History of HMI and Software Versions)
    • What software is on my Parker/CTC HMIs?
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • Gearheads+
  • AC/DC Industrial Drives+
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
Is there a Windows7 / Windows 10 driver for my PHM / PM1 touchscreen interface?

Print Friendly and PDF

NOTE: CDs are no longer shipped with these products. Downloading them from the links provides you with the latest drivers available for your OS.

Yes, there are drivers for the PHM. The TSHARC driver (Ver 6.20cs) that we include on the PHM CD is a legacy driver that supports Win2K and WinXP and it does work with Win7.

Additional Options:

Microchip has newer TSHARC drivers such as the (UniWinDriver 7.08) that will support WinXP and Win7, but not Win2K. It should also support Windows 10. We have not yet officially qualified this latest driver, nor do we include it on the CD. In addition to the UniWinDriver, there is a newer Touchbase UPDD driver also available. 

In the mean time, customers can download the latest drivers here, under the "TSHARC Drivers and Driver Manuals" tab:

https://www.microchip.com/design-centers/tsharc/software-drivers-and-driver-manuals

No for the PM1. The UPDD driver we have for the PM1 does not work in Windows 7 or beyond. The PM1 was only in production and sold during the time Windows XP was available and the version we are licensed to distribute is only for Windows XP. To use a PM1 with Windows 7 and newer, you will need to purchase a new driver from Touchbase licensed for your required OS.

The Touchbase website has versions for various OS versions and you can buy the new driver and get it delivered electronically from Touchbase.

https://www.touch-base.com/drivers

glh 2014 Mar

glh Mar 2014

dom May 2019

dcliffe 28JUN2019 Updated link.

dom July 2019 - No CDs included

  • Touchscreen
  • PHM
  • Windows 10
  • Windows 7
  • Windows XP
  • PM1
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply