Home Technologies Electromechanical Group Electromechanical - Industrial Electromechanical Industrial Knowledge Base IEC Error Message: No valid license for the current hardware
Electromechanical - Industrial
  • Technologies
  • Electromechanical Group
  • Electromechanical - Industrial
  • More
  • Cancel
Electromechanical - Industrial
Electromechanical Industrial Knowledge Base IEC Error Message: No valid license for the current hardware
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
  • Motion and Machine Controllers-
    • ACR Controllers-
      • 7000+
      • ACROBasic Programming (IPA/7000/9000)+
      • 9000 (Legacy)+
      • IEC PLC (9600) (Legacy)-
        • Acrobasic commands for IEC PLC
        • ACRView 6.4.1 Runtime Error for 9600 and 9640
        • ACRView IEC Editor not Compatible with Win10
        • Converting ACR9600 Projects to ACR9000 Projects
        • General Function Block Behavior
        • How to add multiple outputs in ACR IEC PLC ladder programs
        • How to change the Task Type or Task Speed
        • How to change velocity on the fly
        • How to home to a limit in ACR96xx
        • How to Modify a ACR-View project (9600) AcroBasic only programs for Win10
        • How to run an AcroBasic program from IEC PLC
        • How to start the IEC PLC on controller power-up
        • How to use Direct Variable references in ACR IEC PLC
        • IEC Error Message: No valid license for the current hardware
        • Invert Motion Direction in IEC PLC
        • Is there a First Scan flag in the IEC PLC
        • PLCOpen State Machine
        • Set Compax3-EPL Current Limit
        • User Function Block : Excess Position Error Response
        • User Function Block : Moving Average
        • User Function Block : Rotary Axis Position
        • User Function Block: Read Actual Torque
        • User Function Block: Software Limits
        • Using arrays in IEC PLC
        • Using the IEC Debug Window and Watch Lists
        • Variable Declarations in IEC Languages
        • VIDEO: How to import function blocks into ACR IEC_PLC projects
        • What is a Moving Segment Error?
        • Why is the IEC PLC making the axis to move farther and faster than programmed?
      • PC Card Controllers (Discontinued)+
    • PAC120+
    • PAC340+
    • PAC320 (Discontinued)+
    • 6K (Discontinued)+
  • General Technology Information+
  • Virtual Engineer+
  • Visualization and Human Machine Interface (HMI)+
  • Servo Drives and Servo Drive/Controllers+
  • Stepper Drives and Stepper Drive/Controller+
  • AC/DC Industrial Drives+
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
IEC Error Message: No valid license for the current hardware

Print Friendly and PDF

No valid licence for the current hardware module.

No valid license for the current hardware module.

This error occurs when installing a previous version of ACR-View6. The IEC license expires  every January. After that time, a newer version of ACR-View6 is released with a new license. It is available as a free download on our website.

Jan 2018 update:

The ACR 9600 series of controllers are a legacy product and enabled users to program using both AcroBasic and IEC 61131-3 code. Users of the ACR9600 family who utilize the IEC 61131-3 should still upgrade to 6.4.2 to benefit from the various bug fixes; however, the IEC 61131-3 editor capabilities of ACRView are only available on Windows 7.
Users who want to use Windows 10 and IEC 61131-3 should consider migrating to the PAC (Parker Automation Controller), see http://parker.com/emn/pac

Note: ACR9600 controllers can use ACRView 9000 projects (or AcroBasic-only projects) and in these cases, use Windows 8 and 10 if desired.

2/5/18jh update

11/14jh

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply